Data structure of the boot event.
Public Attribute Documentation#
major#
uint16_t sl_bt_evt_system_boot_s::major
Major release version
Definition at line
999
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
minor#
uint16_t sl_bt_evt_system_boot_s::minor
Minor release version
Definition at line
1000
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
patch#
uint16_t sl_bt_evt_system_boot_s::patch
Patch release number
Definition at line
1001
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
build#
uint16_t sl_bt_evt_system_boot_s::build
Build number
Definition at line
1002
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
bootloader#
uint32_t sl_bt_evt_system_boot_s::bootloader
Bootloader version if a bootloader is present in the application. Set to 0 if bootloader is not present.
Definition at line
1003
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
hw#
uint16_t sl_bt_evt_system_boot_s::hw
Hardware type: the major chip revision number in the most significant byte and the minor revision in the least significant byte
Definition at line
1005
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
hash#
uint32_t sl_bt_evt_system_boot_s::hash
Version hash
Definition at line
1008
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h