Extended Advertising Configuration Flags#

This enum defines configuration flags for the extended advertising.

Macro Definition Documentation#

SL_BT_EXTENDED_ADVERTISER_ANONYMOUS_ADVERTISING#

#define SL_BT_EXTENDED_ADVERTISER_ANONYMOUS_ADVERTISING
Value:
0x1

Omit advertiser's address from all PDUs (anonymous advertising). The advertising cannot be connectable or scannable if this flag is set.


Definition at line 2941 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

SL_BT_EXTENDED_ADVERTISER_INCLUDE_TX_POWER#

#define SL_BT_EXTENDED_ADVERTISER_INCLUDE_TX_POWER
Value:
0x2

Include the TX power in advertising packets.


Definition at line 2944 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h