Battery GATT Service#
Provides battery sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.
Function Documentation#
sl_gatt_service_battery_on_event#
void sl_gatt_service_battery_on_event (sl_bt_msg_t * evt)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Event coming from the Bluetooth stack. | 
Bluetooth stack event handler.
sl_gatt_service_battery_get_level#
uint8_t sl_gatt_service_battery_get_level (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Getter for Battery Level characteristic value. Returns
- Battery charge level percent (0..100). 
Note
- To be implemented in user code. 
sl_gatt_service_battery_get_type#
uint8_t sl_gatt_service_battery_get_type (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Getter for Power Source characteristic value. Returns
- Power source type represented as an integer. 
Note
- To be implemented in user code.