Air Quality GATT Service#
Provides air quality sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.
Functions#
void
sl_gatt_service_gas_on_event(sl_bt_msg_t *evt)
sl_status_t
sl_gatt_service_gas_get(uint16_t *eco2, uint16_t *tvoc)
Function Documentation#
sl_gatt_service_gas_on_event#
void sl_gatt_service_gas_on_event (sl_bt_msg_t * evt)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_msg_t * | [in] | evt | Event coming from the Bluetooth stack. | 
Bluetooth stack event handler.
sl_gatt_service_gas_get#
sl_status_t sl_gatt_service_gas_get (uint16_t * eco2, uint16_t * tvoc)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t * | [out] | eco2 | Equivalent CO2 level (in ppm). | 
| uint16_t * | [out] | tvoc | Total Volatile Organic Compounds level (in ppb). | 
Getter for ECO2 and TVOC characteristic values. Returns
- Status of the operation. 
Note
- To be implemented in user code.