CTE type flags for limiting periodic advertising synchronization#
Defines sync CTE type flags that are used to limit what types of periodic advertisers to sync to when scanning for periodic advertising synchronization or receiving periodic advertising synchronization transfers.
Macro Definition Documentation#
SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOA#
#define SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOAValue:
0x1
Do not sync to packets with an AoA Constant Tone Extension
Definition at line
14704
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_1_US#
#define SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_1_USValue:
0x2
Do not sync to packets with an AoD Constant Tone Extension with 1 us slots
Definition at line
14708
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_2_US#
#define SL_BT_CTE_RECEIVER_DO_NOT_SYNC_TO_AOD_2_USValue:
0x4
Do not sync to packets with an AoD Constant Tone Extension with 2 us slots
Definition at line
14712
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
SL_BT_CTE_RECEIVER_SYNC_TO_CTE_ONLY#
#define SL_BT_CTE_RECEIVER_SYNC_TO_CTE_ONLYValue:
0x10
Do not sync to packets without a Constant Tone Extension
Definition at line
14715
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h