BT Event System Event Masks#
Event Mask values used with Event System.
When the component bluetooth_event_system_ipc
is included in the application, the Bluetooth host stack events are published using the Event System provided by the event_system
component. The constants in this group define the event masks used for Bluetooth host stack events.
Macros#
#define
SL_BT_EVENT_MASK_PUBLIC ((uint32_t) 0x01)
Event mask bit set in all public Bluetooth host events.
Macro Definition Documentation#
SL_BT_EVENT_MASK_PUBLIC#
#define SL_BT_EVENT_MASK_PUBLICValue:
((uint32_t) 0x01)
Event mask bit set in all public Bluetooth host events.
Definition at line
59
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h