Data structure of the scan_request event.
Public Attribute Documentation#
handle#
uint8_t sl_bt_evt_advertiser_scan_request_s::handle
Advertising set handle where the scan request was received
address_type#
uint8_t sl_bt_evt_advertiser_scan_request_s::address_type
Enum sl_bt_gap_address_type_t.
Scanner address type.
If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:
- 0: Public address 
- 1: Random address 
If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:
- sl_bt_gap_public_address (0x0): Public device address 
- sl_bt_gap_static_address (0x1): Static device address 
- sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address 
- sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address 
- sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA) 
- sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA) 
bonding#
uint8_t sl_bt_evt_advertiser_scan_request_s::bonding
Bonding handle if the remote scanning device has previously bonded with the local device. Values:
- SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding 
- Other: Bonding handle