sl_bt_evt_connection_tx_power#
Reports a transmit power change on the local device of a connection if transmit power reporting has been enabled.
Enable or disable transmit power reporting using sl_bt_connection_set_power_reporting command. Local transmit power reporting is enabled by default for new connections.
When enabled, local transmit power change events may get triggered in the following situations:
- When the connection has just opened and the initial transmit power is set 
- When the application explicitly changes the system TX power using the sl_bt_system_set_tx_power command 
- When the bluetooth_feature_power_control component is included and enabled in the application and the local transmit power is adjusted by the power control feature 
- When the bluetooth_feature_afh component for Adaptive Frequency Hopping is included and enabled in the application and the local transmit power is adjusted due to changes in the availability of good channels. 
Modules#
sl_bt_evt_connection_tx_power_s
Typedefs#
Macros#
Identifier of the tx_power event.
Typedef Documentation#
sl_bt_evt_connection_tx_power_t#
typedef struct sl_bt_evt_connection_tx_power_s sl_bt_evt_connection_tx_power_t