sl_bt_evt_external_bondingdb_data#

Indicates that updated bonding data of a connection is available.

The application must store it in the external bonding database permanently.

Modules#

sl_bt_evt_external_bondingdb_data_s

Macros#

#define

Identifier of the data event.

Typedef Documentation#

sl_bt_evt_external_bondingdb_data_t#

typedef struct sl_bt_evt_external_bondingdb_data_s sl_bt_evt_external_bondingdb_data_t

Definition at line 11575 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_external_bondingdb_data_id#

#define sl_bt_evt_external_bondingdb_data_id
Value:
0x015c00a0

Identifier of the data event.


Definition at line 11522 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h