Data structure of the bonded event.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_sm_bonded_s::connection

Connection handle


bonding#

uint8_t sl_bt_evt_sm_bonded_s::bonding

Bonding handle. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): Pairing completed without bonding - the pairing key will be discarded after disconnection.

  • Other: Procedure completed, pairing key stored with given bonding handle


security_mode#

uint8_t sl_bt_evt_sm_bonded_s::security_mode

Enum sl_bt_connection_security_t. Connection security mode. Values:

  • sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption

  • sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption

  • sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key