sl_bt_evt_system_boot#

Indicates that the device has started and the radio is ready.

This event carries the firmware build number and other software and hardware identification codes.

Modules#

sl_bt_evt_system_boot_s

Macros#

#define

Identifier of the boot event.

Typedef Documentation#

sl_bt_evt_system_boot_t#

typedef struct sl_bt_evt_system_boot_s sl_bt_evt_system_boot_t

Definition at line 1011 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_system_boot_id#

#define sl_bt_evt_system_boot_id
Value:
0x000100a0

Identifier of the boot event.


Definition at line 992 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h