sl_bt_evt_test_dtm_completed#
Indicates that the radio has processed a test start or end command.
The result parameter indicates the success of the command.
After the receiver or transmitter test is stopped, the number_of_packets parameter in this event indicates the number of received or transmitted packets. 
Modules#
sl_bt_evt_test_dtm_completed_s
Typedefs#
typedef struct sl_bt_evt_test_dtm_completed_s
Macros#
#define
sl_bt_evt_test_dtm_completed_id 0x000e00a0
Identifier of the dtm_completed event.
Typedef Documentation#
sl_bt_evt_test_dtm_completed_t#
typedef struct sl_bt_evt_test_dtm_completed_s sl_bt_evt_test_dtm_completed_t