Periodic Advertising Configuration Flags#

Defines configuration flags for periodic advertising.

Macro Definition Documentation#

SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER#

#define SL_BT_PERIODIC_ADVERTISER_INCLUDE_TX_POWER
Value:
0x1

Include the TX power in advertising packets.


Definition at line 3233 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING#

#define SL_BT_PERIODIC_ADVERTISER_AUTO_START_EXTENDED_ADVERTISING
Value:
0x2

Automatically start the extended advertising on the advertising set. The advertising will be started in non-connectable and non-scannable mode.


Definition at line 3237 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h