Data structure of the phy_status event.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_connection_phy_status_s::connection

Connection handle


Definition at line 6001 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

phy#

uint8_t sl_bt_evt_connection_phy_status_s::phy

Current active PHY. See values from sl_bt_connection_set_preferred_phy command.


Definition at line 6002 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h