Data structure of the request_subrate_failed event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_request_subrate_failed_s::connection
Connection handle
Definition at line
6364
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
result#
uint16_t sl_bt_evt_connection_request_subrate_failed_s::result
The error code provided by the failed procedure
Definition at line
6365
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h