sl_bt_evt_gatt_descriptor#

Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.

It is generated after issuing the sl_bt_gatt_discover_descriptors or sl_bt_gatt_discover_characteristic_descriptors command.

Modules#

sl_bt_evt_gatt_descriptor_s

Macros#

#define

Identifier of the descriptor event.

Typedef Documentation#

sl_bt_evt_gatt_descriptor_t#

typedef struct sl_bt_evt_gatt_descriptor_s sl_bt_evt_gatt_descriptor_t

Definition at line 7693 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_gatt_descriptor_id#

#define sl_bt_evt_gatt_descriptor_id
Value:
0x030900a0

Identifier of the descriptor event.


Definition at line 7681 of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h