Data structure of the descriptor event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_descriptor_s::connection
Connection handle
Definition at line
7688
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
descriptor#
uint16_t sl_bt_evt_gatt_descriptor_s::descriptor
GATT characteristic descriptor handle
Definition at line
7689
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
uuid#
uint8array sl_bt_evt_gatt_descriptor_s::uuid
Descriptor UUID in little endian format
Definition at line
7690
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h