Data structure of the service event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_service_s::connection
Connection handle
Definition at line
7632
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
service#
uint32_t sl_bt_evt_gatt_service_s::service
GATT service handle
Definition at line
7633
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
uuid#
uint8array sl_bt_evt_gatt_service_s::uuid
Service UUID in little endian format
Definition at line
7634
of file /mnt/raid/workspaces/ws.0UefUd3Ll/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h