Accurate Bluetooth Ranging#
Accurate Bluetooth Ranging.
This class provides commands and events for Accurate Bluetooth Ranging (ABR) between Bluetooth devices.
Modules#
sl_bt_evt_cs_security_enable_complete
sl_bt_evt_cs_procedure_enable_complete
Enumerations#
Specifies the role for the device during ABR procedure.
Defines the status of a given role for an ABR capable device.
Defines the status of a companion signal.
Defines the ABR procedure state for the device.
Defines the different modes for ABR steps.
Defines the Round Trip Time (RTT) payload types used during the ABR sequence.
Specifies the ABR channel selection algorithms.
Specifies the ch3c shapes.
Describes the current status of the procedure or subevents.
Describes the abort reasons for ABR procedures and subevents and is represented by 4 bits in a byte.
Specifies the role for the device during ABR procedure.
Functions#
Macros#
Enumeration Documentation#
sl_bt_cs_role_t#
sl_bt_cs_role_t
Specifies the role for the device during ABR procedure.
Enumerator | |
---|---|
sl_bt_cs_role_initiator | |
sl_bt_cs_role_reflector |
12441
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_role_status_t#
sl_bt_cs_role_status_t
Defines the status of a given role for an ABR capable device.
Enumerator | |
---|---|
sl_bt_cs_role_status_disable | |
sl_bt_cs_role_status_enable |
12452
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_companion_signal_status_t#
sl_bt_cs_companion_signal_status_t
Defines the status of a companion signal.
Enumerator | |
---|---|
sl_bt_cs_companion_signal_status_disable | |
sl_bt_cs_companion_signal_status_enable |
12461
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_procedure_state_t#
sl_bt_cs_procedure_state_t
Defines the ABR procedure state for the device.
Enumerator | |
---|---|
sl_bt_cs_procedure_state_disabled | |
sl_bt_cs_procedure_state_enabled |
12472
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_mode_t#
sl_bt_cs_mode_t
Defines the different modes for ABR steps.
Enumerator | |
---|---|
sl_bt_cs_mode_rtt | |
sl_bt_cs_mode_pbr | |
sl_bt_cs_submode_disabled |
12482
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_rtt_type_t#
sl_bt_cs_rtt_type_t
Defines the Round Trip Time (RTT) payload types used during the ABR sequence.
Enumerator | |
---|---|
sl_bt_cs_rtt_type_coarse | |
sl_bt_cs_rtt_type_fractional_96_bit_sounding |
12495
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_channel_selection_algorithm_t#
sl_bt_cs_channel_selection_algorithm_t
Specifies the ABR channel selection algorithms.
Enumerator | |
---|---|
sl_bt_cs_channel_selection_algorithm_3b | |
sl_bt_cs_channel_selection_algorithm_3c | |
sl_bt_cs_channel_selection_algorithm_user_shape_interleaved |
12506
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_ch3c_shape_t#
sl_bt_cs_ch3c_shape_t
Specifies the ch3c shapes.
Enumerator | |
---|---|
sl_bt_cs_ch3c_shape_hat | |
sl_bt_cs_chc3_shape_interleaved |
12542
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_done_status_t#
sl_bt_cs_done_status_t
Describes the current status of the procedure or subevents.
Enumerator | |
---|---|
sl_bt_cs_done_status_complete | |
sl_bt_cs_done_status_partial_results_continue | |
sl_bt_cs_done_status_current_aborted | |
sl_bt_cs_done_status_all_aborted |
12553
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_abort_reason_t#
sl_bt_cs_abort_reason_t
Describes the abort reasons for ABR procedures and subevents and is represented by 4 bits in a byte.
Enumerator | |
---|---|
sl_bt_cs_abort_reason_no_abort | |
sl_bt_cs_abort_reason_host_request | |
sl_bt_cs_abort_reason_insufficient_channels | |
sl_bt_cs_abort_reason_no_map_update | |
sl_bt_cs_abort_reason_unspecified |
12575
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_config_state_t#
sl_bt_cs_config_state_t
Specifies the role for the device during ABR procedure.
Enumerator | |
---|---|
sl_bt_cs_config_state_removed | |
sl_bt_cs_config_state_created |
12593
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Function Documentation#
sl_bt_cs_security_enable#
sl_status_t sl_bt_cs_security_enable (uint8_t connection)
[in] | connection | Connection handle |
Start or restart ABR security start procedure for the specified connection.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_security_enable_complete - Triggered when ABR security start procedure has completed.
13070
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_set_default_settings#
sl_status_t sl_bt_cs_set_default_settings (uint8_t connection, uint8_t initiator_status, uint8_t reflector_status, uint8_t antenna_identifier, int8_t max_tx_power)
[in] | connection | Connection handle |
[in] | initiator_status | Enum sl_bt_cs_role_status_t. Enable or disable status of the Initiator role. Values:
|
[in] | reflector_status | Enum sl_bt_cs_role_status_t. Enable or disable status of the Reflector role. Values:
|
[in] | antenna_identifier | Antenna identifier to be used for ABR sync packets.
|
[in] | max_tx_power | Maximum transmit power level to be used in all ABR transmissions. Units: dBm.
|
Set the default ABR settings for the specified connection. By default, all roles are disabled and the antenna is set to 1.
Returns
SL_STATUS_OK if successful. Error code otherwise.
13096
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_create_config#
sl_status_t sl_bt_cs_create_config (uint8_t connection, uint8_t config_id, uint8_t create_context, uint8_t main_mode_type, uint8_t sub_mode_type, uint8_t min_main_mode_steps, uint8_t max_main_mode_steps, uint8_t main_mode_repetition, uint8_t mode_calibration_steps, uint8_t role, uint8_t rtt_type, uint8_t cs_sync_phy, const sl_bt_cs_channel_map_t *channel_map, uint8_t channel_map_repetition, uint8_t channel_selection_type, uint8_t ch3c_shape, uint8_t ch3c_jump, uint8_t companion_signal_state)
[in] | connection | The connection handle |
[in] | config_id | ABR configuration identifier.
|
[in] | create_context | Defines in which device the created configuration will be written
|
[in] | main_mode_type | Enum sl_bt_cs_mode_t. Main mode type. Values:
|
[in] | sub_mode_type | Enum sl_bt_cs_mode_t. Sub mode type. Values:
|
[in] | min_main_mode_steps | Minimum number of ABR main mode steps to be executed prior to a sub mode step.
|
[in] | max_main_mode_steps | Maximum number of ABR main mode steps to be executed prior to a sub mode step.
|
[in] | main_mode_repetition | Number of main mode steps taken from the end of the last ABR subevent to be repeated at the beginning of the current ABR subevent directly after the value r last Mode 0 step of that event.
|
[in] | mode_calibration_steps | Number of Mode 0 steps to be included at the beginning of the test ABR subevent
|
[in] | role | Enum sl_bt_cs_role_t. Device's role during the ABR procedure Values:
|
[in] | rtt_type | Enum sl_bt_cs_rtt_type_t. RTT payload type used in the ABR procedure Values:
|
[in] | cs_sync_phy | Enum sl_bt_gap_phy_t. Used PHY for ABR SYNC exchanges during a procedure Values:
|
[in] | channel_map | A fixed length byte array of 10 bytes consisting of 79 1-bit fields. The nth such field (in the range 0 to 78) contains the value for the ABR channel index n.
The rest of most significant bits are reserved for future use and must be set to 0. Channels n = 0, 1, 23, 24, 25, 77 and 78 shall be ignored and not used for ABR. At least 15 channels shall be marked as used. |
[in] | channel_map_repetition | Number of times the channel_map field will be cycled through for non-Mode 0 steps within an ABR procedure.
|
[in] | channel_selection_type | Enum sl_bt_cs_channel_selection_algorithm_t. Channel selection algorithm Values:
|
[in] | ch3c_shape | Enum sl_bt_cs_ch3c_shape_t. Ch3c shape Values:
|
[in] | ch3c_jump | Number of channels skipped in each rising and falling sequence.
|
[in] | companion_signal_state | Enum sl_bt_cs_companion_signal_status_t. Companion device's signal status Values:
|
Create a new ABR configuration in the local and remote controller. The role used in this command must be enabled prior to issuing this command using sl_bt_cs_set_default_settings command.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_config_complete - Triggered when an ABR configuration procedure completed
13200
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_remove_config#
sl_status_t sl_bt_cs_remove_config (uint8_t connection, uint8_t config_id)
[in] | connection | Connection handle |
[in] | config_id | ABR configuration identifier
|
Remove an ABR configuration from the local controller.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_config_complete - Triggered when an ABR configuration procedure is completed
13234
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_set_channel_classification#
sl_status_t sl_bt_cs_set_channel_classification (const sl_bt_cs_channel_map_t *channel_map)
[in] | channel_map | A fixed length byte array of 10 bytes consisting of 79 1-bit fields. The nth field (in the range 0 to 78) contains the value for the link layer channel index n.
The rest of most significant bits are reserved for future use and must be set to 0. Channels n = 0, 1, 23, 24, 25, 77 and 78 shall be ignored and not used for ABR. |
Update the channel classification for ABR. This classification persists until overwritten with a subsequent command or until the system is reset.
Returns
SL_STATUS_OK if successful. Error code otherwise.
13258
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_set_procedure_parameters#
sl_status_t sl_bt_cs_set_procedure_parameters (uint8_t connection, uint8_t config_id, uint16_t max_procedure_len, uint16_t min_procedure_interval, uint16_t max_procedure_interval, uint16_t max_procedure_count, uint32_t min_subevent_len, uint32_t max_subevent_len, uint8_t tone_antenna_config_selection, uint8_t phy, int8_t tx_pwr_delta, uint8_t preferred_peer_antenna)
[in] | connection | The connection handle |
[in] | config_id | ABR configuration identifier.
|
[in] | max_procedure_len | Maximum duration for each measurement procedure. Value in units of 0.625 ms.
|
[in] | min_procedure_interval | Minimum duration in number of connection events between consecutive measurement procedure.
|
[in] | max_procedure_interval | Maximum duration in number of connection events between consecutive measurement procedure.
|
[in] | max_procedure_count | Maximum number of ABR procedures to be scheduled
|
[in] | min_subevent_len | Minimum suggested duration for each ABR subevent. Units: microseconds.
|
[in] | max_subevent_len | Maximum suggested duration for each ABR subevent. Units: microseconds.
|
[in] | tone_antenna_config_selection | Antenna configuration index
|
[in] | phy | Enum sl_bt_gap_phy_t. PHY on which the ABR transmission will take place Values:
|
[in] | tx_pwr_delta | Transmit power delta. Units: dB.
|
[in] | preferred_peer_antenna | Preferred peer-ordered antenna elements to be used by the remote device for the antenna configuration denoted by the tone antenna config selection.
|
Set the parameters for scheduling ABR procedures with the remote device.
Returns
SL_STATUS_OK if successful. Error code otherwise.
13312
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_procedure_enable#
sl_status_t sl_bt_cs_procedure_enable (uint8_t connection, uint8_t enable, uint8_t config_id)
[in] | connection | The connection handle |
[in] | enable | Enum sl_bt_cs_procedure_state_t. Enabled or disabled ABR procedure state. Values:
|
[in] | config_id | ABR configuration identifier |
Enable or disable scheduling ABR procedures with the remote device.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_cs_procedure_enable_complete - Triggered when local controller has scheduled or disabled an ABR procedure measurement
sl_bt_evt_cs_result - Triggered when local controller has results to report for every ABR event within the ABR procedure
13347
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_set_antenna_configuration#
sl_status_t sl_bt_cs_set_antenna_configuration (size_t antenna_element_offset_len, const uint8_t *antenna_element_offset)
[in] | antenna_element_offset_len | Length of data in |
[in] | antenna_element_offset | Offset of each antenna, each element is a signed 16-bit integer stored in two consecutive bytes in little-endian order. Units: 1 cm. |
Set the antenna configuration for the ABR feature.
Returns
SL_STATUS_OK if successful. Error code otherwise.
13364
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cs_read_local_supported_capabilities#
sl_status_t sl_bt_cs_read_local_supported_capabilities (uint8_t *num_config, uint16_t *max_consecutive_procedures, uint8_t *num_antennas, uint8_t *max_antenna_paths, uint8_t *roles, uint8_t *optional_modes, uint8_t *rtt_capability, uint8_t *rtt_aa_only, uint8_t *rtt_sounding, uint8_t *rtt_random_payload, uint8_t *optional_cs_sync_phys, uint16_t *optional_subfeatures, uint16_t *optional_t_ip1_times, uint16_t *optional_t_ip2_times, uint16_t *optional_t_fcs_times, uint16_t *optional_t_pm_times, uint8_t *t_sw_times)
[out] | num_config | The number of ABR configurations supported per connection.
|
[out] | max_consecutive_procedures | The maximum number of consecutive ABR procedures supported.
|
[out] | num_antennas | The number of antenna elements available for ABR tone exchanges.
|
[out] | max_antenna_paths | The maximum number of antenna paths supported.
|
[out] | roles | This value is a bitmask of flags to indicate which ABR roles are supported by the controller. Flags:
|
[out] | optional_modes | This value is a bitmask of flags to indicate which Optional ABR modes are supported. Flags:
|
[out] | rtt_capability | This value is a bitmask of flags to indicate which Round Trip Time (RTT) ABR capabilities accuracy requirement in
|
[out] | rtt_aa_only | RTT Access Address(AA) is supported by the controller
|
[out] | rtt_sounding | RTT Sounding is supported by the controller
|
[out] | rtt_random_payload | RTT Random Payload is supported by the controller
|
[out] | optional_cs_sync_phys | This value is a bitmask of flags to indicate which ABR SYNC packages supported in an specific PHY. Flags:
|
[out] | optional_subfeatures | This value is a bitmask of flags to indicate which Optional ABR subfeatures supported is supported. Flags:
|
[out] | optional_t_ip1_times | This value is a bitmask of flags to indicate which Time for Interlude Period 1 (IP1) supported is supported. Flags:
|
[out] | optional_t_ip2_times | This value is a bitmask of flags to indicate which Time for Interlude Period 2 (IP2) supported is supported. Flags:
|
[out] | optional_t_fcs_times | This value is a bitmask of flags to indicate which Time for Frequency Change Spaceing (FCS) is supported. Flags:
|
[out] | optional_t_pm_times | This value is a bitmask of flags to indicate which Time for Phase Measurement (PM) supported is supported. Flags:
|
[out] | t_sw_times | Time in microseconds for the antenna switch period of the ABR tones.
|
Read the ABR capabilities of the local controller.
Returns
SL_STATUS_OK if successful. Error code otherwise.
13465
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_cmd_cs_security_enable_id#
#define sl_bt_cmd_cs_security_enable_idValue:
0x00590020
12419
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_set_default_settings_id#
#define sl_bt_cmd_cs_set_default_settings_idValue:
0x01590020
12420
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_create_config_id#
#define sl_bt_cmd_cs_create_config_idValue:
0x02590020
12421
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_remove_config_id#
#define sl_bt_cmd_cs_remove_config_idValue:
0x03590020
12422
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_set_channel_classification_id#
#define sl_bt_cmd_cs_set_channel_classification_idValue:
0x04590020
12423
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_set_procedure_parameters_id#
#define sl_bt_cmd_cs_set_procedure_parameters_idValue:
0x05590020
12424
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_procedure_enable_id#
#define sl_bt_cmd_cs_procedure_enable_idValue:
0x06590020
12425
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_set_antenna_configuration_id#
#define sl_bt_cmd_cs_set_antenna_configuration_idValue:
0x07590020
12426
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_cmd_cs_read_local_supported_capabilities_id#
#define sl_bt_cmd_cs_read_local_supported_capabilities_idValue:
0x08590020
12427
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_security_enable_id#
#define sl_bt_rsp_cs_security_enable_idValue:
0x00590020
12428
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_set_default_settings_id#
#define sl_bt_rsp_cs_set_default_settings_idValue:
0x01590020
12429
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_create_config_id#
#define sl_bt_rsp_cs_create_config_idValue:
0x02590020
12430
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_remove_config_id#
#define sl_bt_rsp_cs_remove_config_idValue:
0x03590020
12431
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_set_channel_classification_id#
#define sl_bt_rsp_cs_set_channel_classification_idValue:
0x04590020
12432
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_set_procedure_parameters_id#
#define sl_bt_rsp_cs_set_procedure_parameters_idValue:
0x05590020
12433
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_procedure_enable_id#
#define sl_bt_rsp_cs_procedure_enable_idValue:
0x06590020
12434
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_set_antenna_configuration_id#
#define sl_bt_rsp_cs_set_antenna_configuration_idValue:
0x07590020
12435
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
sl_bt_rsp_cs_read_local_supported_capabilities_id#
#define sl_bt_rsp_cs_read_local_supported_capabilities_idValue:
0x08590020
12436
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h