Connection#

Connection.

The commands and events in this class are related to managing connection establishment, parameter setting, and disconnection procedures.

Modules#

RSSI Value Constants

Transmit Power Reporting Constants

sl_bt_evt_connection_opened

sl_bt_evt_connection_parameters

sl_bt_evt_connection_set_parameters_failed

sl_bt_evt_connection_phy_status

sl_bt_evt_connection_get_remote_tx_power_completed

sl_bt_evt_connection_tx_power

sl_bt_evt_connection_remote_tx_power

sl_bt_evt_connection_remote_used_features

sl_bt_evt_connection_data_length

sl_bt_evt_connection_statistics

sl_bt_evt_connection_request_subrate_failed

sl_bt_evt_connection_subrate_changed

sl_bt_evt_connection_channel_classification

sl_bt_evt_connection_closed

Enumerations#

enum
sl_bt_connection_role_peripheral = 0x0
sl_bt_connection_role_central = 0x1
}

Types of device roles in a Bluetooth connection.

enum
sl_bt_connection_state_closed = 0x0
sl_bt_connection_state_closing = 0x1
sl_bt_connection_state_open = 0x2
sl_bt_connection_state_opening = 0x3
}

Connection states.

enum
sl_bt_connection_mode1_level1 = 0x0
sl_bt_connection_mode1_level2 = 0x1
sl_bt_connection_mode1_level3 = 0x2
sl_bt_connection_mode1_level4 = 0x3
}

Indicate the Bluetooth Security Mode.

enum
sl_bt_connection_power_reporting_disable = 0x0
sl_bt_connection_power_reporting_enable = 0x1
}

These values define transmit power reporting modes in LE power control.

enum
sl_bt_connection_tx_power_flag_none = 0x0
sl_bt_connection_tx_power_at_minimum = 0x1
sl_bt_connection_tx_power_at_maximum = 0x2
}

This enum defines the flag values for a reported transmit power level.

Functions#

sl_status_t
sl_bt_connection_set_default_parameters(uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length)
sl_status_t
sl_bt_connection_set_default_preferred_phy(uint8_t preferred_phy, uint8_t accepted_phy)
sl_status_t
sl_status_t
sl_bt_connection_set_default_acceptable_subrate(uint16_t min_subrate, uint16_t max_subrate, uint16_t max_latency, uint16_t continuation_number, uint16_t max_timeout)
sl_status_t
sl_bt_connection_open(bd_addr address, uint8_t address_type, uint8_t initiating_phy, uint8_t *connection)
sl_status_t
sl_bt_connection_open_with_accept_list(uint8_t initiating_phy, uint8_t *connection)
sl_status_t
sl_bt_connection_set_parameters(uint8_t connection, uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length)
sl_status_t
sl_bt_connection_set_preferred_phy(uint8_t connection, uint8_t preferred_phy, uint8_t accepted_phy)
sl_status_t
sl_bt_connection_disable_slave_latency(uint8_t connection, uint8_t disable)
sl_status_t
sl_bt_connection_get_median_rssi(uint8_t connection, int8_t *rssi)
sl_status_t
sl_bt_connection_read_channel_map(uint8_t connection, size_t max_channel_map_size, size_t *channel_map_len, uint8_t *channel_map)
sl_status_t
sl_bt_connection_set_power_reporting(uint8_t connection, uint8_t mode)
sl_status_t
sl_bt_connection_set_remote_power_reporting(uint8_t connection, uint8_t mode)
sl_status_t
sl_bt_connection_get_tx_power(uint8_t connection, uint8_t phy, int8_t *current_level, int8_t *max_level)
sl_status_t
sl_bt_connection_get_remote_tx_power(uint8_t connection, uint8_t phy)
sl_status_t
sl_bt_connection_set_tx_power(uint8_t connection, int16_t tx_power, int16_t *tx_power_out)
sl_status_t
sl_status_t
sl_bt_connection_get_security_status(uint8_t connection, uint8_t *security_mode, uint8_t *key_size, uint8_t *bonding_handle)
sl_status_t
sl_bt_connection_set_data_length(uint8_t connection, uint16_t tx_data_len, uint16_t tx_time_us)
sl_status_t
sl_bt_connection_read_statistics(uint8_t connection, uint8_t reset)
sl_status_t
sl_bt_connection_get_scheduling_details(uint8_t connection, uint32_t *access_address, uint8_t *role, uint32_t *crc_init, uint16_t *interval, uint16_t *supervision_timeout, uint8_t *central_clock_accuracy, uint8_t *central_phy, uint8_t *peripheral_phy, uint8_t *channel_selection_algorithm, uint8_t *hop, sl_bt_connection_channel_map_t *channel_map, uint8_t *channel, uint16_t *event_counter, uint32_t *start_time_us)
sl_status_t
sl_bt_connection_get_remote_address(uint8_t connection, bd_addr *address, uint8_t *address_type)
sl_status_t
sl_bt_connection_request_subrate(uint8_t connection, uint16_t min_subrate, uint16_t max_subrate, uint16_t max_latency, uint16_t continuation_number, uint16_t timeout)
sl_status_t
sl_bt_connection_get_state(uint8_t connection, uint8_t *state)
sl_status_t
sl_bt_connection_close(uint8_t connection)
sl_status_t

Macros#

#define
sl_bt_cmd_connection_set_default_parameters_id 0x00060020
#define
sl_bt_cmd_connection_set_default_preferred_phy_id 0x01060020
#define
sl_bt_cmd_connection_set_default_data_length_id 0x10060020
#define
sl_bt_cmd_connection_set_default_acceptable_subrate_id 0x19060020
#define
sl_bt_cmd_connection_open_id 0x04060020
#define
sl_bt_cmd_connection_open_with_accept_list_id 0x16060020
#define
sl_bt_cmd_connection_set_parameters_id 0x06060020
#define
sl_bt_cmd_connection_set_preferred_phy_id 0x08060020
#define
sl_bt_cmd_connection_disable_slave_latency_id 0x03060020
#define
sl_bt_cmd_connection_get_median_rssi_id 0x15060020
#define
sl_bt_cmd_connection_read_channel_map_id 0x07060020
#define
sl_bt_cmd_connection_set_power_reporting_id 0x09060020
#define
sl_bt_cmd_connection_set_remote_power_reporting_id 0x0a060020
#define
sl_bt_cmd_connection_get_tx_power_id 0x0b060020
#define
sl_bt_cmd_connection_get_remote_tx_power_id 0x0c060020
#define
sl_bt_cmd_connection_set_tx_power_id 0x12060020
#define
sl_bt_cmd_connection_read_remote_used_features_id 0x0d060020
#define
sl_bt_cmd_connection_get_security_status_id 0x0e060020
#define
sl_bt_cmd_connection_set_data_length_id 0x11060020
#define
sl_bt_cmd_connection_read_statistics_id 0x13060020
#define
sl_bt_cmd_connection_get_scheduling_details_id 0x14060020
#define
sl_bt_cmd_connection_get_remote_address_id 0x17060020
#define
sl_bt_cmd_connection_request_subrate_id 0x1a060020
#define
sl_bt_cmd_connection_get_state_id 0x18060020
#define
sl_bt_cmd_connection_close_id 0x05060020
#define
sl_bt_cmd_connection_forcefully_close_id 0x0f060020
#define
sl_bt_rsp_connection_set_default_parameters_id 0x00060020
#define
sl_bt_rsp_connection_set_default_preferred_phy_id 0x01060020
#define
sl_bt_rsp_connection_set_default_data_length_id 0x10060020
#define
sl_bt_rsp_connection_set_default_acceptable_subrate_id 0x19060020
#define
sl_bt_rsp_connection_open_id 0x04060020
#define
sl_bt_rsp_connection_open_with_accept_list_id 0x16060020
#define
sl_bt_rsp_connection_set_parameters_id 0x06060020
#define
sl_bt_rsp_connection_set_preferred_phy_id 0x08060020
#define
sl_bt_rsp_connection_disable_slave_latency_id 0x03060020
#define
sl_bt_rsp_connection_get_median_rssi_id 0x15060020
#define
sl_bt_rsp_connection_read_channel_map_id 0x07060020
#define
sl_bt_rsp_connection_set_power_reporting_id 0x09060020
#define
sl_bt_rsp_connection_set_remote_power_reporting_id 0x0a060020
#define
sl_bt_rsp_connection_get_tx_power_id 0x0b060020
#define
sl_bt_rsp_connection_get_remote_tx_power_id 0x0c060020
#define
sl_bt_rsp_connection_set_tx_power_id 0x12060020
#define
sl_bt_rsp_connection_read_remote_used_features_id 0x0d060020
#define
sl_bt_rsp_connection_get_security_status_id 0x0e060020
#define
sl_bt_rsp_connection_set_data_length_id 0x11060020
#define
sl_bt_rsp_connection_read_statistics_id 0x13060020
#define
sl_bt_rsp_connection_get_scheduling_details_id 0x14060020
#define
sl_bt_rsp_connection_get_remote_address_id 0x17060020
#define
sl_bt_rsp_connection_request_subrate_id 0x1a060020
#define
sl_bt_rsp_connection_get_state_id 0x18060020
#define
sl_bt_rsp_connection_close_id 0x05060020
#define
sl_bt_rsp_connection_forcefully_close_id 0x0f060020

Enumeration Documentation#

sl_bt_connection_role_t#

sl_bt_connection_role_t

Types of device roles in a Bluetooth connection.

Enumerator
sl_bt_connection_role_peripheral

(0x0) The Peripheral role

sl_bt_connection_role_central

(0x1) The Central role


sl_bt_connection_state_t#

sl_bt_connection_state_t

Connection states.

Enumerator
sl_bt_connection_state_closed

(0x0) Connection closed

sl_bt_connection_state_closing

(0x1) Connection is being closed

sl_bt_connection_state_open

(0x2) Connection open

sl_bt_connection_state_opening

(0x3) Connection is being opened


sl_bt_connection_security_t#

sl_bt_connection_security_t

Indicate the Bluetooth Security Mode.

Enumerator
sl_bt_connection_mode1_level1

(0x0) No security

sl_bt_connection_mode1_level2

(0x1) Unauthenticated pairing with encryption

sl_bt_connection_mode1_level3

(0x2) Authenticated pairing with encryption

sl_bt_connection_mode1_level4

(0x3) Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key


sl_bt_connection_power_reporting_mode_t#

sl_bt_connection_power_reporting_mode_t

These values define transmit power reporting modes in LE power control.

Enumerator
sl_bt_connection_power_reporting_disable

(0x0) Disable transmit power reporting

sl_bt_connection_power_reporting_enable

(0x1) Enable transmit power reporting


sl_bt_connection_tx_power_flag_t#

sl_bt_connection_tx_power_flag_t

This enum defines the flag values for a reported transmit power level.

Enumerator
sl_bt_connection_tx_power_flag_none

(0x0) No flag is defined for the reported TX power level

sl_bt_connection_tx_power_at_minimum

(0x1) Transmit power level is at minimum level.

sl_bt_connection_tx_power_at_maximum

(0x2) Transmit power level is at maximum level.


Function Documentation#

sl_bt_connection_set_default_parameters#

sl_status_t sl_bt_connection_set_default_parameters (uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]min_interval

Minimum value for the connection event interval. This must be set less than or equal to max_interval.

  • Range: 0x0006 to 0x0c80

  • Time = Value x 1.25 ms

  • Time Range: 7.5 ms to 4 s

  • Default : 20 ms

uint16_t[in]max_interval

Maximum value for the connection event interval. This must be set greater than or equal to min_interval.

  • Range: 0x0006 to 0x0c80

  • Time = Value x 1.25 ms

  • Time Range: 7.5 ms to 4 s

  • Default : 50 ms

uint16_t[in]latency

Peripheral latency, which defines how many connection intervals the peripheral can skip if it has no data to send

  • Range: 0x0000 to 0x01f3

  • Default : 0

uint16_t[in]timeout

Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.

  • Range: 0x000a to 0x0c80

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + latency) * max_interval * 2, where max_interval is given in milliseconds

Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.

  • Default : 1000 ms

uint16_t[in]min_ce_length

Minimum length of the connection event. It must be less than or equal to max_ce_length.

This value defines the minimum time that should be given to the connection event in a situation where other tasks need to run immediately after the connection event. When the value is very small, the connection event still has at least one TX/RX operation. If this value is increased, more time is reserved for the connection event so it can transmit and receive more packets in a connection interval.

Use the default value if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

  • Default : 0x0000

uint16_t[in]max_ce_length

Maximum length of the connection event. It must be greater than or equal to min_ce_length.

This value is used for limiting the connection event length so that a connection that has large amounts of data to transmit or receive doesn't block other tasks. Limiting the connection event is a hard stop. If there is no enough time to send or receive a packet, the connection event will be closed.

If the value is set to 0, the connection event still has at least one TX/RX operation. This is useful to limit power consumption or leave more time to other tasks.

Use the default value if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

  • Default : 0xffff

Set default Bluetooth connection parameters. The values are valid for all subsequent connections initiated by this device.

min_ce_length and max_ce_length specify the preference of the connection event length so that the Link Layer can prioritize tasks accordingly in simultaneous connections, or scanning and so on. A connection event starts at an anchor point of a connection interval and lasts until the lesser of max_ce_length and the actual connection interval. Packets that do not fit into the connection event will be sent in the next connection interval.

To change parameters of an already established connection, use the command sl_bt_connection_set_parameters.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_set_default_preferred_phy#

sl_status_t sl_bt_connection_set_default_preferred_phy (uint8_t preferred_phy, uint8_t accepted_phy)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]preferred_phy

Preferred PHYs. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: Coded PHY

  • 0xff: Any PHYs

Default: 0xff (no preference)

uint8_t[in]accepted_phy

Accepted PHYs in remotely-initiated PHY update request. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: Coded PHY

  • 0xff: Any PHYs

Default: 0xff (all PHYs accepted)

Set default preferred and accepted PHYs. PHY settings will be used for all subsequent connections. Non-preferred PHY can also be set if the remote device does not accept any of the preferred PHYs.

The parameter accepted_phy is used to specify PHYs that the stack can accept in a remotely-initiated PHY update request. A PHY update will not happen if none of the accepted PHYs are present in the request.

NOTE: 2M and Coded PHYs are not supported by all devices.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_set_default_data_length#

sl_status_t sl_bt_connection_set_default_data_length (uint16_t tx_data_len)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]tx_data_len

Preferred maximum payload octets of a packet that the local Controller will send

  • Range: 0x001B to 0x00FB

  • Default : 251

Set the default preferred maximum TX payload length to be used for new connections.

When a connection is open, the maximum TX payload length is 27. Either device could initiate a data length update procedure and event sl_bt_evt_connection_data_length is generated when the data length has been changed on the connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_set_default_acceptable_subrate#

sl_status_t sl_bt_connection_set_default_acceptable_subrate (uint16_t min_subrate, uint16_t max_subrate, uint16_t max_latency, uint16_t continuation_number, uint16_t max_timeout)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]min_subrate

Minimum subrate factor allowed in requests by a peripheral. This parameter must be set to less or equal to max_subrate.

  • Range: 1 to 500

  • Default : 1

uint16_t[in]max_subrate

Maximum subrate factor allowed in requests by a peripheral. This parameter must be set greater or equal to min_subrate.

  • Range: 1 to 500

  • Default : 1

uint16_t[in]max_latency

Maximum Peripheral latency allowed in requests, in units of subrated connection intervals. The result of (max_latency + 1) x max_subrate must be less than or equal to 500.

  • Range: 0 to 499

  • Default : 0

uint16_t[in]continuation_number

Minimum number of underlying connection events to remain active after a packet containing a Controller PDU with a non-zero Length field is sent or received in requests by a peripheral. This number must be set to be smaller than max_subrate.

  • Range: 0 to 499

  • Default : 0

uint16_t[in]max_timeout

Maximum supervision timeout allowed in requests by a peripheral.

  • Range: 10 (100 ms) to 3200 (32 s)

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • Default : 10 (100 ms)

Set the default acceptable parameters for subrating requests made by the peripheral on future ACL connections where this device is the central. The application must include the Connection Subrating feature (bluetooth_feature_connection_subrating) in order to use this command.

When a connection is established, central will store these values to determine if future subrate requests from the peripheral are acceptable. Peripheral may store it's own set of parameters independently but they will not be used in that role. Running this command has no effect on connections that are already active, instead to change the stored acceptable values, use the command sl_bt_connection_request_subrate on the central device.

Subrating is not automatically enabled on new a connection. Use the command sl_bt_connection_request_subrate to set the subrate parameters and enable subrating of a specific connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_open#

sl_status_t sl_bt_connection_open (bd_addr address, uint8_t address_type, uint8_t initiating_phy, uint8_t * connection)
Parameters
TypeDirectionArgument NameDescription
bd_addr[in]address

Address of the device to connect to

uint8_t[in]address_type

Enum sl_bt_gap_address_type_t. Address type of the device to connect to. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)

uint8_t[in]initiating_phy

Enum sl_bt_gap_phy_t. The initiating PHY. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)

uint8_t *[out]connection

Handle that will be assigned to the connection after the connection is established. This handle is valid only if the result code of this response is 0 (zero).

Connect to an advertising device with the specified initiating PHY on which connectable advertisements on primary advertising channels are received. The Bluetooth stack will enter a state where it continuously scans for the connectable advertising packets from the remote device, which matches the Bluetooth address given as a parameter. Scan parameters set in sl_bt_scanner_set_parameters are used in this operation. Upon receiving the advertising packet, the module will send a connection request packet to the target device to initiate a Bluetooth connection. To cancel an ongoing connection process, use sl_bt_connection_close command with the handle received in response from this command.

If privacy is enabled, see sl_bt_gap_set_privacy_mode for the initiator private address behavior.

A connection is opened in no-security mode. If the GATT client needs to read or write the attributes on GATT server requiring encryption or authentication, it must first encrypt the connection using an appropriate authentication method.

If a connection can't be established, for example, the remote device has gone out of range, has entered into deep sleep, or is not advertising, the stack will try to connect forever. In this case, the application will not get an event related to the connection request. To recover from this situation, the application can implement a timeout and call sl_bt_connection_close to cancel the connection request.

This command fails with the connection limit exceeded error if the number of connections attempted exceeds the configured MAX_CONNECTIONS value.

This command fails with the invalid parameter error if the initiating PHY value is invalid or the device does not support PHY.

Subsequent calls of this command have to wait for the ongoing command to complete. A received event sl_bt_evt_connection_opened indicates that the connection opened successfully and a received event sl_bt_evt_connection_closed indicates that connection failures have occurred.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events

  • sl_bt_evt_connection_opened - This event is triggered after the connection is opened and indicates whether the devices are already bonded and the role of the device in this connection.

  • sl_bt_evt_connection_parameters - This event indicates the connection parameters and security mode of the connection.


sl_bt_connection_open_with_accept_list#

sl_status_t sl_bt_connection_open_with_accept_list (uint8_t initiating_phy, uint8_t * connection)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]initiating_phy

Enum sl_bt_gap_phy_t. The initiating PHY. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)

uint8_t *[out]connection

Handle that will be assigned to the connection after the connection is established. This handle is valid only if the result code of this response is 0 (zero).

Connect to any device in the Filter Accept List, which enables the Auto Connection Establishment procedure on the local controller. The behavior of this command is the same as sl_bt_connection_open. The only difference is that sl_bt_connection_open opens a connection to a given peer device address.

See sl_bt_connection_open for more details.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events

  • sl_bt_evt_connection_opened - This event is triggered after the connection is opened and indicates whether the devices are already bonded and the role of the device in this connection.

  • sl_bt_evt_connection_parameters - This event indicates the connection parameters and security mode of the connection.


sl_bt_connection_set_parameters#

sl_status_t sl_bt_connection_set_parameters (uint8_t connection, uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection Handle

uint16_t[in]min_interval

Minimum value for the connection event interval. This must be set less than or equal to max_interval.

  • Range: 0x0006 to 0x0c80

  • Time = Value x 1.25 ms

  • Time Range: 7.5 ms to 4 s

uint16_t[in]max_interval

Maximum value for the connection event interval. This must be set greater than or equal to min_interval.

  • Range: 0x0006 to 0x0c80

  • Time = Value x 1.25 ms

  • Time Range: 7.5 ms to 4 s

uint16_t[in]latency

Peripheral latency, which defines how many connection intervals the peripheral can skip if it has no data to send

  • Range: 0x0000 to 0x01f3

uint16_t[in]timeout

Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.

  • Range: 0x000a to 0x0c80

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + latency) * max_interval * 2, where max_interval is given in milliseconds

Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.

uint16_t[in]min_ce_length

Minimum length of the connection event. It must be less than or equal to max_ce_length.

This value defines the minimum time that should be given to the connection event in a situation where other tasks need to run immediately after the connection event. When the value is very small, the connection event still has at least one TX/RX operation. If this value is increased, more time is reserved for the connection event so it can transmit and receive more packets in a connection interval.

Use value 0x0000 if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

uint16_t[in]max_ce_length

Maximum length of the connection event. It must be greater than or equal to min_ce_length.

This value is used for limiting the connection event length so that a connection that has large amounts of data to transmit or receive doesn't block other tasks. Limiting the connection event is a hard stop. If there is no enough time to send or receive a packet, the connection event will be closed.

If the value is set to 0, the connection event still has at least one TX/RX operation. This is useful to limit power consumption or leave more time to other tasks.

Use value 0xffff if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

Request a change in the connection parameters of a Bluetooth connection.

  • On the central device the HCI LE Connection Update command is used to update the parameters.

  • On the peripheral device an L2CAP connection parameter update request is sent to the peer device to update the parameters.

min_ce_length and max_ce_length specify the preference of the connection event length so that the Link Layer can prioritize tasks accordingly in simultaneous connections, or scanning and so on. A connection event starts at an anchor point of a connection interval and lasts until the lesser of max_ce_length and the actual connection interval. Packets that do not fit into the connection event will be sent in the next connection interval.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_set_preferred_phy#

sl_status_t sl_bt_connection_set_preferred_phy (uint8_t connection, uint8_t preferred_phy, uint8_t accepted_phy)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint8_t[in]preferred_phy

Preferred PHYs. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: 125k Coded PHY (S=8)

  • 0x08: 500k Coded PHY (S=2)

Default: 0xff (no preference)

uint8_t[in]accepted_phy

Accepted PHYs in remotely-initiated PHY update requests. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: Coded PHY

  • 0xff: Any PHYs

Default: 0xff (all PHYs accepted)

Set preferred and accepted PHYs for a given connection. Event sl_bt_evt_connection_phy_status is received when PHY update procedure is completed. Non-preferred PHY can also be set if remote device does not accept any of the preferred PHYs.

The parameter accepted_phy is used for specifying the PHYs that the stack can accept in a remote initiated PHY update request. A PHY update will not occur if none of the accepted PHYs presents in the request.

NOTE: 2M and Coded PHYs are not supported by all devices.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_disable_slave_latency#

sl_status_t sl_bt_connection_disable_slave_latency (uint8_t connection, uint8_t disable)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection Handle

uint8_t[in]disable

0 enable, 1 disable peripheral latency. Default: 0

Temporarily enable or disable peripheral latency. Used only when Bluetooth device is acting as a peripheral. When peripheral latency is disabled, the peripheral latency connection parameter is not set to 0 but the device will wake up on every connection interval to receive and send packets.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_get_median_rssi#

sl_status_t sl_bt_connection_get_median_rssi (uint8_t connection, int8_t * rssi)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

int8_t *[out]rssi

The median of the last seven measured RSSI values. Units: dBm.

  • Range: -127 to +20

Get the RSSI value measured on a connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_read_channel_map#

sl_status_t sl_bt_connection_read_channel_map (uint8_t connection, size_t max_channel_map_size, size_t * channel_map_len, uint8_t * channel_map)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection Handle

size_t[in]max_channel_map_size

Size of output buffer passed in channel_map

size_t *[out]channel_map_len

On return, set to the length of output data written to channel_map

uint8_t *[out]channel_map

This parameter is 5 bytes and contains 37 1-bit fields.

The nth field (in the range 0 to 36) contains the value for the link layer channel index n.

  • 0: Channel n is unused.

  • 1: Channel n is used.

The most significant bits are reserved for future use.

Read channel map for a specified connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_set_power_reporting#

sl_status_t sl_bt_connection_set_power_reporting (uint8_t connection, uint8_t mode)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Handle of the connection

uint8_t[in]mode

Enum sl_bt_connection_power_reporting_mode_t. Transmit power reporting mode. Values:

  • sl_bt_connection_power_reporting_disable (0x0): Disable transmit power reporting

  • sl_bt_connection_power_reporting_enable (0x1): Enable transmit power reporting

Enable or disable the transmit power reporting for the local device on a connection. When transmit power reporting is enabled, event sl_bt_evt_connection_tx_power is generated when transmit power on the local device changes.

The command is a built-in feature in the stack and is supported regardless of whether the LE Power Control feature is used. By default, power reporting for local device is enabled.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_set_remote_power_reporting#

sl_status_t sl_bt_connection_set_remote_power_reporting (uint8_t connection, uint8_t mode)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Handle of the connection

uint8_t[in]mode

Enum sl_bt_connection_power_reporting_mode_t. Transmit power reporting mode. Values:

  • sl_bt_connection_power_reporting_disable (0x0): Disable transmit power reporting

  • sl_bt_connection_power_reporting_enable (0x1): Enable transmit power reporting

Enable or disable reporting the transmit power change on the remote device. The application must include the LE Power Control feature (bluetooth_feature_power_control) in order to use this command.

When the remote transmit power reporting is enabled, event sl_bt_evt_connection_remote_tx_power is generated when transmit power on the remote device changes.

By default, power reporting for the remote device is disabled.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_get_tx_power#

sl_status_t sl_bt_connection_get_tx_power (uint8_t connection, uint8_t phy, int8_t * current_level, int8_t * max_level)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Handle of the connection

uint8_t[in]phy

Enum sl_bt_gap_phy_coding_t. The PHY. Values:

  • sl_bt_gap_phy_coding_1m_uncoded (0x1): 1M PHY

  • sl_bt_gap_phy_coding_2m_uncoded (0x2): 2M PHY

  • sl_bt_gap_phy_coding_125k_coded (0x4): 125k Coded PHY (S=8)

  • sl_bt_gap_phy_coding_500k_coded (0x8): 500k Coded PHY (S=2)

int8_t *[out]current_level

The current transmit power level in dBm of the PHY on the connection. Values:

int8_t *[out]max_level

The maximum transmit power level in dBm of the PHY on the connection.

  • Range: -127 to +20

Get the transmit power of the local device on the given connection and PHY. The application must include the LE Power Control feature (bluetooth_feature_power_control) in order to use this command.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_get_remote_tx_power#

sl_status_t sl_bt_connection_get_remote_tx_power (uint8_t connection, uint8_t phy)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Handle of the connection

uint8_t[in]phy

Enum sl_bt_gap_phy_coding_t. The PHY. Values:

  • sl_bt_gap_phy_coding_1m_uncoded (0x1): 1M PHY

  • sl_bt_gap_phy_coding_2m_uncoded (0x2): 2M PHY

  • sl_bt_gap_phy_coding_125k_coded (0x4): 125k Coded PHY (S=8)

  • sl_bt_gap_phy_coding_500k_coded (0x8): 500k Coded PHY (S=2)

Get the transmit power of the remote device on the given connection and PHY. The application must include the LE Power Control feature (bluetooth_feature_power_control) in order to use this command. Transmit power levels are returned in event sl_bt_evt_connection_get_remote_tx_power_completed after the operation completed.

Returns

  • SL_STATUS_OK if the command is accepted. Error code otherwise.

Events


sl_bt_connection_set_tx_power#

sl_status_t sl_bt_connection_set_tx_power (uint8_t connection, int16_t tx_power, int16_t * tx_power_out)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

The connection handle

int16_t[in]tx_power

The requested TX power. Unit: 0.1 dBm

int16_t *[out]tx_power_out

The selected TX power. Unit: 0.1 dBm

Set the transmit power of a connection. The application must include component bluetooth_feature_user_power_control in order to use this command for controlling the transmit power of the connection at application level. This command is unavailable if the standard Bluetooth feature LE power control (component bluetooth_feature_power_control) is used by the application.

The actual selected power level is returned from this command. The value may be different than the requested one because of system-wide TX power setting by the application, Bluetooth feature restrictions, or radio characteristics.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_read_remote_used_features#

sl_status_t sl_bt_connection_read_remote_used_features (uint8_t connection)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection Handle

Read link layer features supported by the remote device.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_get_security_status#

sl_status_t sl_bt_connection_get_security_status (uint8_t connection, uint8_t * security_mode, uint8_t * key_size, uint8_t * bonding_handle)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint8_t *[out]security_mode

Enum sl_bt_connection_security_t. Connection security mode. Values:

  • sl_bt_connection_mode1_level1 (0x0): No security

  • sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption

  • sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption

  • sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key

uint8_t *[out]key_size

The size of encryption key

uint8_t *[out]bonding_handle

Bonding handle. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle

Get the security status of the connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_set_data_length#

sl_status_t sl_bt_connection_set_data_length (uint8_t connection, uint16_t tx_data_len, uint16_t tx_time_us)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint16_t[in]tx_data_len

Preferred maximum payload octets of a packet that the local Controller will send

  • Range: 20 (0x1B) to 251 (0XFB)

uint16_t[in]tx_time_us

Preferred maximum TX time in microseconds that the local Controller will take to send a packet

  • Range: 328 (0x0148) to 17040 (0x4290)

Request to update the maximum TX payload length and maximum packet TX time of a Bluetooth connection.

Event sl_bt_evt_connection_data_length is generated when the data length has been changed on the connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_read_statistics#

sl_status_t sl_bt_connection_read_statistics (uint8_t connection, uint8_t reset)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

The connection handle

uint8_t[in]reset

Reset statistics if parameter value is not zero

Read the statistic values collected on the specified connection. The application must include component bluetooth_feature_connection_statistics in order to use this command. If the component is not included in the application this command returns the error SL_STATUS_NOT_AVAILABLE. If this command is called before the connection has opened, the command returns the error SL_STATUS_NOT_READY.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_get_scheduling_details#

sl_status_t sl_bt_connection_get_scheduling_details (uint8_t connection, uint32_t * access_address, uint8_t * role, uint32_t * crc_init, uint16_t * interval, uint16_t * supervision_timeout, uint8_t * central_clock_accuracy, uint8_t * central_phy, uint8_t * peripheral_phy, uint8_t * channel_selection_algorithm, uint8_t * hop, sl_bt_connection_channel_map_t * channel_map, uint8_t * channel, uint16_t * event_counter, uint32_t * start_time_us)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint32_t *[out]access_address

Access address of the connection

uint8_t *[out]role

Enum sl_bt_connection_role_t. The role the local device operates in the connection. Values:

  • sl_bt_connection_role_peripheral (0x0): The Peripheral role

  • sl_bt_connection_role_central (0x1): The Central role

uint32_t *[out]crc_init

The CRC initialization value

uint16_t *[out]interval

The connection interval. Time = Value x 1.25 ms

uint16_t *[out]supervision_timeout

The connection supervision time. Time = Value x 10 ms

uint8_t *[out]central_clock_accuracy

The central device's clock accuracy index value

uint8_t *[out]central_phy

Enum sl_bt_gap_phy_t. The PHY that the Central device is transmitting on. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_2m (0x2): 2M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)

uint8_t *[out]peripheral_phy

Enum sl_bt_gap_phy_t. The PHY that the Peripheral device is transmitting on. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_2m (0x2): 2M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)

uint8_t *[out]channel_selection_algorithm

Enum sl_bt_gap_channel_selection_algorithm_t. The channel selection algorithm. Values:

  • sl_bt_gap_channel_selection_algorithm_1 (0x0): Channel selection algorithm #1

  • sl_bt_gap_channel_selection_algorithm_2 (0x1): Channel selection algorithm #2

uint8_t *[out]hop

The hop increment when the channel selection algorithm #1 is used on the connection. Ignore if channel_selection_algorithm indicates that the connection uses channel selection algorithm #2.

sl_bt_connection_channel_map_t *[out]channel_map

5 byte bit field in little endian format. Only the first 37 bits are used. Bit 0 of the first byte is channel 0, bit 0 of the second byte is channel 8, etc. Ignore bits 37-39 that are reserved for future use.

A channel is unused when its bit is 0. A channel is used when its bit is 1.

uint8_t *[out]channel

The data channel number that transmissions will use in the next connection event

uint16_t *[out]event_counter

The event counter of the next connection event

uint32_t *[out]start_time_us

Time in microseconds from the PROTIMER tick when the next connection event is scheduled to happen

Get parameters and next connection event scheduling details of a connection. Returned values from this command provide the necessary information for following the packet transmissions of the connection on an external device. Note that the stack cannot ensure a determined timing latency from the time when issuing this command to the time when another device starts to follow the connection, and the stack cannot guarantee that a scheduled connection event will always happen.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_get_remote_address#

sl_status_t sl_bt_connection_get_remote_address (uint8_t connection, bd_addr * address, uint8_t * address_type)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

bd_addr *[out]address

Bluetooth address of the remote device

uint8_t *[out]address_type

Enum sl_bt_gap_address_type_t. Remote device address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)

Get the Bluetooth address of the remote device on the given connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_request_subrate#

sl_status_t sl_bt_connection_request_subrate (uint8_t connection, uint16_t min_subrate, uint16_t max_subrate, uint16_t max_latency, uint16_t continuation_number, uint16_t timeout)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint16_t[in]min_subrate

Minimum subrate factor to be applied to the underlying connection interval. This parameter must be set to less or equal to max_subrate.

  • Range: 1 to 500

  • Default : 1

uint16_t[in]max_subrate

Maximum subrate factor to be applied to the underlying connection interval. This parameter must be set greater or equal to min_subrate.

  • Range: 1 to 500

  • Default : 1

uint16_t[in]max_latency

Maximum Peripheral latency for the connection in units of subrated connection intervals. The result of (max_latency + 1) x max_subrate must be less than or equal to 500.

  • Range: 0 to 499

  • Default : 0

uint16_t[in]continuation_number

Minimum number of underlying connection events to remain active after a packet containing a Link Layer PDU with a non-zero Length field is sent or received. This number must be set to be smaller than max_subrate.

  • Range: 0 to 499

  • Default : 0

uint16_t[in]timeout

Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.

  • Range: 10 (100 ms) to 3200 (32 s)

  • Default : 10 (100 ms)

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + max_latency) * factor * max_interval * 1.25 * 2. The factor is max_subrate if the central requests the subrating, or min_subrate if the peripheral requests the subrating.

Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.

Request a change to the subrating factor and other parameters applied to an existing connection. The application must include the Connection Subrating feature (bluetooth_feature_connection_subrating) in order to use this command.

If the local device is in the central role on this connection, this command overrides the default acceptable subrating parameters set by sl_bt_connection_set_default_acceptable_subrate and uses the specified subrate parameters for this connection. If the local device is in the peripheral role on this connection, this command requests a change to the parameters but they may not be accepted by the peer central device.

If the connection parameters are changed (see command sl_bt_connection_set_parameters and event sl_bt_evt_connection_parameters) after subrate parameters were successfully applied, the latency and timeout from sl_bt_evt_connection_parameters take effect and the subrate_factor is reset to 1 and the continuation_number to 0 for the connection. Use this command sl_bt_connection_request_subrate again after the connection parameter change to re-enable subrating.

This command returns SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATURE when the device is in central role on the connection and the peripheral does not support the subrate feature.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_get_state#

sl_status_t sl_bt_connection_get_state (uint8_t connection, uint8_t * state)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint8_t *[out]state

Enum sl_bt_connection_state_t. State of the given connection. Values:

  • sl_bt_connection_state_closed (0x0): Connection closed

  • sl_bt_connection_state_closing (0x1): Connection is being closed

  • sl_bt_connection_state_open (0x2): Connection open

  • sl_bt_connection_state_opening (0x3): Connection is being opened

Get the state of the given connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_connection_close#

sl_status_t sl_bt_connection_close (uint8_t connection)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Handle of the connection to be closed

Close a Bluetooth connection gracefully by performing the ACL Termination procedure or cancel an ongoing connection establishment process. The parameter is a connection handle which is reported in sl_bt_evt_connection_opened event or sl_bt_connection_open command response.

Disconnecting a connection is an asynchronous operation. The disconnection is completed when a sl_bt_evt_connection_closed event for the given connection handle is received. To open a new connection to the same remote device, wait for the sl_bt_evt_connection_closed event and then initiate the connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_connection_forcefully_close#

sl_status_t sl_bt_connection_forcefully_close (uint8_t connection)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Handle of the connection to be closed

Forcefully close a Bluetooth connection without performing the ACL Termination procedure. The parameter is a connection handle which is reported in sl_bt_evt_connection_opened event or sl_bt_connection_open command response.

Closing a connection using this command could result in the observation of connection loss or supervision timeout on the remote device. Only use this command for special cases, for example, when disconnecting a connection with sl_bt_connection_close did not complete in expected time period.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events