sl_bt_evt_connection_get_remote_tx_power_completed#

Indicates that reading remote transmit power initiated by sl_bt_connection_get_remote_tx_power command has completed.

Modules#

sl_bt_evt_connection_get_remote_tx_power_completed_s

Macros#

#define

Identifier of the get_remote_tx_power_completed event.

Typedef Documentation#

sl_bt_evt_connection_get_remote_tx_power_completed_t#

typedef struct sl_bt_evt_connection_get_remote_tx_power_completed_s sl_bt_evt_connection_get_remote_tx_power_completed_t

Definition at line 5761 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_connection_get_remote_tx_power_completed_id#

#define sl_bt_evt_connection_get_remote_tx_power_completed_id
Value:
0x050600a0

Identifier of the get_remote_tx_power_completed event.


Definition at line 5710 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h