Bluetooth Mesh Health Client Model#
Bluetooth Mesh Health Client Model.
This class provides the commands and messages to interface with the Health Client model.
Modules#
sl_btmesh_evt_health_client_server_status
sl_btmesh_evt_health_client_server_status_period
sl_btmesh_evt_health_client_server_status_attention
Functions#
Macros#
Function Documentation#
sl_btmesh_health_client_init#
sl_status_t sl_btmesh_health_client_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize health client.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_health_client_deinit#
sl_status_t sl_btmesh_health_client_deinit (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Deinitialize health client.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_health_client_get#
sl_status_t sl_btmesh_health_client_get (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint16_t vendor_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address. May be a unicast address or a group address. |
| uint16_t | [in] | elem_index | Client model element index. Identifies the client model used for sending the request. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request |
| uint16_t | [in] | vendor_id | Bluetooth vendor ID used in the request |
Get the registered fault status of a Health Server model or models in the network.
Besides the immediate result code, the response or responses (if the destination server address is a group address) from the network will generate sl_btmesh_evt_health_client_server_status.
Returns
If an error occurs locally, (for instance, because of invalid parameters) an errorcode parameter is returned immediately.
Events
sl_btmesh_health_client_clear#
sl_status_t sl_btmesh_health_client_clear (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint16_t vendor_id, uint8_t reliable)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address. May be a unicast address or a group address. |
| uint16_t | [in] | elem_index | Client model element index. Identifies the client model used for sending the request. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request |
| uint16_t | [in] | vendor_id | Bluetooth vendor ID used in the request |
| uint8_t | [in] | reliable | If non-zero, a reliable model message is used. |
Clear the fault status of a Health Server model or models in the network.
Besides the immediate result code, the response or responses (if the destination server address is a group address) from the network will generate sl_btmesh_evt_health_client_server_status.
Returns
If an error occurs locally (for instance, because of invalid parameters), an errorcode parameter is returned immediately.
Events
sl_btmesh_health_client_test#
sl_status_t sl_btmesh_health_client_test (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint8_t test_id, uint16_t vendor_id, uint8_t reliable)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address. May be a unicast address or a group address. |
| uint16_t | [in] | elem_index | Client model element index. Identifies the client model used for sending the request. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request |
| uint8_t | [in] | test_id | Test ID used in the request |
| uint16_t | [in] | vendor_id | Bluetooth vendor ID used in the request |
| uint8_t | [in] | reliable | If non-zero, a reliable model message is used. |
Execute a self test on a server model or models in the network.
Returns
If an error occurs locally (for instance, because of invalid parameters) an errorcode parameter is returned immediately.
Events
sl_btmesh_health_client_get_period#
sl_status_t sl_btmesh_health_client_get_period (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address, which may be a unicast address or a group address |
| uint16_t | [in] | elem_index | Client model element index. Identifies the client model used for sending the request. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request |
Get the health period log of a Health Server model or models in the network.
Except for the immediate result code, the response or responses (if the destination server address is a group address) from the network will generate sl_btmesh_evt_health_client_server_status_period.
Returns
If an error occurs locally, (for instance, because of invalid parameters) an errorcode parameter is returned immediately.
Events
sl_btmesh_health_client_set_period#
sl_status_t sl_btmesh_health_client_set_period (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint8_t period, uint8_t reliable)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address. May be a unicast address or a group address. |
| uint16_t | [in] | elem_index | Client model element index, which identifies the client model used for sending the request. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request |
| uint8_t | [in] | period | Health period divisor value. Valid range: 0 - 16. |
| uint8_t | [in] | reliable | If non-zero, a reliable model message is used. |
Set the health period divisor of a Health Server model or models in the network.
Except for the immediate result code, the response or responses (if the destination server address is a group address) from the network will generate sl_btmesh_evt_health_client_server_status_period.
Returns
If an error occurs locally (for instance, because of invalid parameters), an errorcode parameter is returned immediately.
Events
sl_btmesh_health_client_get_attention#
sl_status_t sl_btmesh_health_client_get_attention (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address. May be a unicast address or a group address. |
| uint16_t | [in] | elem_index | Client model element index. Identifies the client model used for sending the request. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request |
Get the attention timer value of a Health Server model or models in the network.
Besides the immediate result code, the response or responses (if the destination server address is a group address) from the network will generate sl_btmesh_evt_health_client_server_status_attention.
Returns
If an error occurs locally (for instance, because of invalid parameters), an errorcode parameter is returned immediately.
Events
sl_btmesh_health_client_set_attention#
sl_status_t sl_btmesh_health_client_set_attention (uint16_t server_address, uint16_t elem_index, uint16_t appkey_index, uint8_t attention_sec, uint8_t reliable)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | server_address | Destination server model address. May be a unicast address or a group address. |
| uint16_t | [in] | elem_index | Client model element index. Identifies the client model used for sending the request. |
| uint16_t | [in] | appkey_index | The application key index to use in encrypting the request |
| uint8_t | [in] | attention_sec | Attention timer period in seconds |
| uint8_t | [in] | reliable | If non-zero, a reliable model message is used. |
Set the attention timer value of a Health Server model or models in the network.
Except for the immediate result code, the response or responses (if the destination server address is a group address) from the network will generate sl_btmesh_evt_health_client_server_status_attention.
Returns
If an error occurs locally (for instance, because of invalid parameters), an errorcode parameter is returned immediately.
Events