Bluetooth Mesh On-demand Private Proxy Server Model#
Bluetooth Mesh On-demand Private Proxy Server Model.
The On-Demand Private Proxy Server model is used to support the configuration of the advertising with Private Network Identity type functionality of a node. Requires the presence of the corresponding Solicitation PDU RPL Configuration Server model, which is initialized with it at the same time (see init command).
Macros#
#define
sl_btmesh_cmd_on_demand_private_proxy_server_init_id 0x016a0028
#define
sl_btmesh_cmd_on_demand_private_proxy_server_deinit_id 0x026a0028
#define
sl_btmesh_rsp_on_demand_private_proxy_server_init_id 0x016a0028
#define
sl_btmesh_rsp_on_demand_private_proxy_server_deinit_id 0x026a0028
Function Documentation#
sl_btmesh_on_demand_private_proxy_server_init#
sl_status_t sl_btmesh_on_demand_private_proxy_server_init (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize the On-Demand Private Proxy Server model, and the Solicitation PDU RPL Configuration Server model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_on_demand_private_proxy_server_deinit#
sl_status_t sl_btmesh_on_demand_private_proxy_server_deinit (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Deinitialize the On-Demand Private Proxy Server model, and the Solicitation PDU RPL Configuration Server model
Returns
SL_STATUS_OK if successful. Error code otherwise.