Bluetooth Mesh Private Beacon Client Model#
Bluetooth Mesh Private Beacon Client Model.
This class provides the commands and messages to interface with the Private Beacon Client Model.
Modules#
sl_btmesh_evt_private_beacon_client_beacon_status
sl_btmesh_evt_private_beacon_client_gatt_proxy_status
sl_btmesh_evt_private_beacon_client_identity_status
Functions#
Macros#
Function Documentation#
sl_btmesh_private_beacon_client_init#
sl_status_t sl_btmesh_private_beacon_client_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initialize the private beacon client.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_private_beacon_client_deinit#
sl_status_t sl_btmesh_private_beacon_client_deinit (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Deinitialize the private beacon client.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_private_beacon_client_get_beacon#
sl_status_t sl_btmesh_private_beacon_client_get_beacon (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
| uint16_t | [in] | server_address | Destination node primary element address |
| uint32_t * | [out] | handle | Request handle. |
Get the node's private network beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_private_beacon_client_set_beacon#
sl_status_t sl_btmesh_private_beacon_client_set_beacon (uint16_t enc_netkey_index, uint16_t server_address, uint8_t state, uint16_t random_update_steps, uint32_t * handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
| uint16_t | [in] | server_address | Destination node primary element address |
| uint8_t | [in] | state | Secure network beacon value to set. Valid values are:
|
| uint16_t | [in] | random_update_steps | Number of beacons that are to be sent before changing the random of obfuscation. Valid step values are from 0x00 to 0xff. 0x00 means that the random is updated for every beacon send. and 0x01-0xff tells how often random is updated in multiples of 10 seconds. Update of random will also trigger update of random address used in sending. Value 0x100 is used to indicate that no change in this parameter is desired. |
| uint32_t * | [out] | handle | Request handle |
Set node private network beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_private_beacon_client_get_gatt_proxy#
sl_status_t sl_btmesh_private_beacon_client_get_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
| uint16_t | [in] | server_address | Destination node primary element address |
| uint32_t * | [out] | handle | Request handle. |
Get the node's private gatt proxy beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_private_beacon_client_set_gatt_proxy#
sl_status_t sl_btmesh_private_beacon_client_set_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint8_t state, uint32_t * handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
| uint16_t | [in] | server_address | Destination node primary element address |
| uint8_t | [in] | state | Secure network beacon value to set. Valid values are:
|
| uint32_t * | [out] | handle | Request handle |
Set the node's private gatt proxy beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_private_beacon_client_get_identity#
sl_status_t sl_btmesh_private_beacon_client_get_identity (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint32_t * handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
| uint16_t | [in] | server_address | Destination node primary element address |
| uint16_t | [in] | netkey_index | Network key index for which the state is queried |
| uint32_t * | [out] | handle | Request handle. |
Get the node's private identity beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_private_beacon_client_set_identity#
sl_status_t sl_btmesh_private_beacon_client_set_identity (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint8_t state, uint32_t * handle)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
| uint16_t | [in] | server_address | Destination node primary element address |
| uint16_t | [in] | netkey_index | Network key index for which the state is configured |
| uint8_t | [in] | state | Node private beacon value to set. Valid values are:
|
| uint32_t * | [out] | handle | Request handle |
Set the node's private node identity beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
Macro Definition Documentation#
sl_btmesh_cmd_private_beacon_client_init_id#
#define sl_btmesh_cmd_private_beacon_client_init_idValue:
0x01640028
sl_btmesh_cmd_private_beacon_client_deinit_id#
#define sl_btmesh_cmd_private_beacon_client_deinit_idValue:
0x02640028
sl_btmesh_cmd_private_beacon_client_get_beacon_id#
#define sl_btmesh_cmd_private_beacon_client_get_beacon_idValue:
0x03640028
sl_btmesh_cmd_private_beacon_client_set_beacon_id#
#define sl_btmesh_cmd_private_beacon_client_set_beacon_idValue:
0x04640028
sl_btmesh_cmd_private_beacon_client_get_gatt_proxy_id#
#define sl_btmesh_cmd_private_beacon_client_get_gatt_proxy_idValue:
0x05640028
sl_btmesh_cmd_private_beacon_client_set_gatt_proxy_id#
#define sl_btmesh_cmd_private_beacon_client_set_gatt_proxy_idValue:
0x06640028
sl_btmesh_cmd_private_beacon_client_get_identity_id#
#define sl_btmesh_cmd_private_beacon_client_get_identity_idValue:
0x07640028
sl_btmesh_cmd_private_beacon_client_set_identity_id#
#define sl_btmesh_cmd_private_beacon_client_set_identity_idValue:
0x08640028
sl_btmesh_rsp_private_beacon_client_init_id#
#define sl_btmesh_rsp_private_beacon_client_init_idValue:
0x01640028
sl_btmesh_rsp_private_beacon_client_deinit_id#
#define sl_btmesh_rsp_private_beacon_client_deinit_idValue:
0x02640028
sl_btmesh_rsp_private_beacon_client_get_beacon_id#
#define sl_btmesh_rsp_private_beacon_client_get_beacon_idValue:
0x03640028
sl_btmesh_rsp_private_beacon_client_set_beacon_id#
#define sl_btmesh_rsp_private_beacon_client_set_beacon_idValue:
0x04640028
sl_btmesh_rsp_private_beacon_client_get_gatt_proxy_id#
#define sl_btmesh_rsp_private_beacon_client_get_gatt_proxy_idValue:
0x05640028
sl_btmesh_rsp_private_beacon_client_set_gatt_proxy_id#
#define sl_btmesh_rsp_private_beacon_client_set_gatt_proxy_idValue:
0x06640028
sl_btmesh_rsp_private_beacon_client_get_identity_id#
#define sl_btmesh_rsp_private_beacon_client_get_identity_idValue:
0x07640028
sl_btmesh_rsp_private_beacon_client_set_identity_id#
#define sl_btmesh_rsp_private_beacon_client_set_identity_idValue:
0x08640028