Data structure of the query_block_status_complete event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::elem_index
The client model element index.
block_complete#
uint8_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::block_complete
Non-zero if the block is complete.
transfer_complete#
uint8_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::transfer_complete
Non-zero if the transfer is complete.