Data structure of the identity_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_private_beacon_client_identity_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
status#
uint8_t sl_btmesh_evt_private_beacon_client_identity_status_s::status
Foundation status of last request
netkey_index#
uint16_t sl_btmesh_evt_private_beacon_client_identity_status_s::netkey_index
Network key index for which the state is configured
state#
uint8_t sl_btmesh_evt_private_beacon_client_identity_status_s::state
Private identity beacon state of the node. Valid values are:
0: Node is not broadcasting private identity beacons
1: Node is broadcasting private identity beacons