Data structure of the publish event.

Public Attributes#

uint16_t
uint32_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_scene_setup_server_publish_s::elem_index

Client model element index


period_ms#

uint32_t sl_btmesh_evt_scene_setup_server_publish_s::period_ms

The current publishing period that can be used to estimate the next tick, e.g., when the state should be reported at higher frequency.