Data structure of the store event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::destination_address

Address of the server or the group address to which it was published.


elem_index#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::elem_index

Index of the element which received the command.


scene_id#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::scene_id

Scene ID


client_address#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::client_address

Device which sent the request.


appkey_index#

uint16_t sl_btmesh_evt_scene_setup_server_store_s::appkey_index

Appkey used by client_address.