sl_btmesh_evt_sensor_setup_server_set_setting_request#

Indicate an incoming Sensor Set Setting request, which can be replied to by sending a Sensor Setting Status message.

Only Setting Set (acknowledged) request is replied directly to the client. In addition, configuration changes must be reported by publishing the new state according to model publishing configuration.

Modules#

sl_btmesh_evt_sensor_setup_server_set_setting_request_s

Macros#

#define

Identifier of the set_setting_request event.

Typedef Documentation#

sl_btmesh_evt_sensor_setup_server_set_setting_request_t#

typedef struct sl_btmesh_evt_sensor_setup_server_set_setting_request_s sl_btmesh_evt_sensor_setup_server_set_setting_request_t

Macro Definition Documentation#

sl_btmesh_evt_sensor_setup_server_set_setting_request_id#

#define sl_btmesh_evt_sensor_setup_server_set_setting_request_id
Value:
0x044800a8

Identifier of the set_setting_request event.