BT Event System Event Masks#

SL_BTMESH_API command declarations.

License#

Copyright 2019 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

Event Mask values used with Event System

When the component bluetooth_event_system_ipc is included in the application, the Bluetooth mesh stack events are published using the Event System provided by the event_system component. The constants in this group define the event masks used for Bluetooth mesh stack events.

Macros#

#define
SL_BTMESH_EVENT_MASK_PUBLIC ((uint32_t) 0x01)

Event mask bit set in all public Bluetooth mesh events.

Macro Definition Documentation#

SL_BTMESH_EVENT_MASK_PUBLIC#

#define SL_BTMESH_EVENT_MASK_PUBLIC
Value:
((uint32_t) 0x01)

Event mask bit set in all public Bluetooth mesh events.