Bluetooth Mesh SAR Configuration Client Model#

Bluetooth Mesh SAR Configuration Client Model.

SAR Configuration Client model, used to configure the behavior of the lower transport layer of a node that that supports the SAR Configuration Server

Modules#

sl_btmesh_evt_sar_config_client_sar_transmitter_status

sl_btmesh_evt_sar_config_client_sar_receiver_status

Functions#

sl_status_t
sl_btmesh_sar_config_client_get_sar_transmitter(uint16_t enc_netkey_index, uint16_t server_address, uint32_t *handle)
sl_status_t
sl_btmesh_sar_config_client_set_sar_transmitter(uint16_t enc_netkey_index, uint16_t server_address, uint8_t segment_interval_step, uint8_t unicast_retrans_count, uint8_t unicast_retrans_wo_progress_count, uint16_t unicast_retrans_interval_step, uint16_t unicast_retrans_interval_increment, uint8_t multicast_retrans_count, uint16_t multicast_retrans_interval_step, uint32_t *handle)
sl_status_t
sl_btmesh_sar_config_client_get_sar_receiver(uint16_t enc_netkey_index, uint16_t server_address, uint32_t *handle)
sl_status_t
sl_btmesh_sar_config_client_set_sar_receiver(uint16_t enc_netkey_index, uint16_t server_address, uint8_t segments_threshold, uint8_t ack_delay_increment, uint32_t discard_timeout, uint8_t segment_interval_step, uint8_t ack_retrans_count, uint32_t *handle)

Function Documentation#

sl_btmesh_sar_config_client_init#

sl_status_t sl_btmesh_sar_config_client_init ()

Initialize the SAR Configuration Client model

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_sar_config_client_deinit#

sl_status_t sl_btmesh_sar_config_client_deinit ()

Deinitialize the SAR Configuration Client model

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_btmesh_sar_config_client_get_sar_transmitter#

sl_status_t sl_btmesh_sar_config_client_get_sar_transmitter (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]enc_netkey_index

Network key used to encrypt the request on the network layer

uint16_t[in]server_address

Destination node primary element address

uint32_t *[out]handle

Request handle

Query the SAR Transmitter state of a node

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_btmesh_sar_config_client_set_sar_transmitter#

sl_status_t sl_btmesh_sar_config_client_set_sar_transmitter (uint16_t enc_netkey_index, uint16_t server_address, uint8_t segment_interval_step, uint8_t unicast_retrans_count, uint8_t unicast_retrans_wo_progress_count, uint16_t unicast_retrans_interval_step, uint16_t unicast_retrans_interval_increment, uint8_t multicast_retrans_count, uint16_t multicast_retrans_interval_step, uint32_t * handle)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]enc_netkey_index

Network key used to encrypt the request on the network layer

uint16_t[in]server_address

Destination node primary element address

uint8_t[in]segment_interval_step

SAR Segment Interval Step

The Segment Interval Step controls the interval between transmissions of segments of a segmented message in milliseconds. The value is the range of 10ms to 160ms in 10ms steps, intermediate values are rounded down to the nearest multiple of 10. Default value is 20ms.

uint8_t[in]unicast_retrans_count

SAR Unicast Retransmissions Count

The SAR Unicast Retransmission Count controls the maximum number of transmissions of segments of segmented messages to a unicast destination. Valid range is 0 - 15, where 0 represents a single transmission. The default value is 7, resulting in 8 transmissions total.

uint8_t[in]unicast_retrans_wo_progress_count

SAR Unicast Retransmissions Without Progress Count

The SAR Unicase Retransmissions Without Progress Count controls the maximum number of retransmissions of segments of segmented messages to a unicast destination without progress (without marking newly marking any segments acknowledged). Valid range is 0 - 15, where 0 represents a single transmission. The default value is 2, resulting in 3 transmissions. The value of this state should be set to a value greater by two or more than the value of the SAR Acknowledgement Retransmissions Count on a peer node. This helps prevent the SAR transmitter from abandoning the SAR prematurely.

uint16_t[in]unicast_retrans_interval_step

SAR Unicast Retransmissions Interval Step

The SAR Unicast Retransmissions Interval Step state controls the minimum interval between retransmissions of segments of a segmented message for a destination that is a unicast address in 25ms steps. Valid range is 25 - 400ms, intermediate values are rounded down to the nearest multiple of 25. Default value is 200ms.

uint16_t[in]unicast_retrans_interval_increment

SAR Unicast Retransmissions Interval Increment

The SAR Unicast Retransmissions Interval Increment state controls the incremental component of the interval between retransmissions of segments of a segmented message for a destination that is a unicast address in 25ms steps. Valid range is 25 - 400ms, intermediate values are rounded down to the nearest multiple of 25. Default value is 50ms.

uint8_t[in]multicast_retrans_count

SAR Multicast Retransmissions Count

The SAR Multicast Retransmissions Count state controls the maximum number of transmissions of segments of segmented messages to a group address or a virtual address. Valid range is 0 - 15, where 0 represents a single transmission. The default value is 1, resulting in 2 transmissions.

uint16_t[in]multicast_retrans_interval_step

SAR Multicast Retransmissions Interval

The SAR Multicast Retransmissions Interval Step state controls the interval between retransmissions of segments of a segmented message for a destination that is a group address or a virtual address in 25ms steps. Valid range is 25-400ms, intermediate values are rounded down to the nearest multiple of 25. Default values is 100ms.

uint32_t *[out]handle

Request handle

Set the SAR Tranmitter state of a node

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_btmesh_sar_config_client_get_sar_receiver#

sl_status_t sl_btmesh_sar_config_client_get_sar_receiver (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]enc_netkey_index

Network key used to encrypt the request on the network layer

uint16_t[in]server_address

Destination node primary element address

uint32_t *[out]handle

Request handle

Query the SAR Receiver state of a node

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_btmesh_sar_config_client_set_sar_receiver#

sl_status_t sl_btmesh_sar_config_client_set_sar_receiver (uint16_t enc_netkey_index, uint16_t server_address, uint8_t segments_threshold, uint8_t ack_delay_increment, uint32_t discard_timeout, uint8_t segment_interval_step, uint8_t ack_retrans_count, uint32_t * handle)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]enc_netkey_index

Network key used to encrypt the request on the network layer

uint16_t[in]server_address

Destination node primary element address

uint8_t[in]segments_threshold

SAR Segments Threshold

The SAR Segments Threshold state represents the size of a segmented message in number of segments above which the Segment Acknowledgment messages are enabled. Valid range is 0 - 31, the default value is 3.

uint8_t[in]ack_delay_increment

SAR Acknowledgment Delay Increment

The SAR Acknowledgment Delay Increment state control the interval between the reception of a new segment of a segmented message for a destination that is a unicast address and the transmission of the Segment Acknowledgment for that message. Valid range is 0 - 7, default is 2.

uint32_t[in]discard_timeout

SAR Discard Timeout

The SAR Discard Timeout state controls the time that the lower transport layer waits after receiving unique segments of a segmented message before discarding that segmented message in 5s steps. Valid range is 5000 - 80000ms, intermediate values are rounded down to the nearest multiple of 5s. The default value is 10000ms.

uint8_t[in]segment_interval_step

SAR Discard Timeout

The SAR Discard Timeout state controls the time that the lower transport layer waits after receiving unique segments of a segmented message before discarding that segmented message in 5s steps. Valid range is 5000 - 80000ms, intermediate values are rounded down to the nearest multiple of 5s. The default value is 10000ms.

uint8_t[in]ack_retrans_count

SAR Acknowledgment Retransmissions Count

The SAR Acknowledgment Retransmissions Count state controls the maximum number of retransmissions of Segment Acknowledgment messages sent by the lower transport layer. Valid range is 0 - 3. The default value is 2, representing 2 retransmissions or 3 in total.

uint32_t *[out]handle

Request handle

Set the SAR Receiver state of a node

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Macro Definition Documentation#

sl_btmesh_cmd_sar_config_client_init_id#

#define sl_btmesh_cmd_sar_config_client_init_id
Value:
0x01620028

sl_btmesh_cmd_sar_config_client_deinit_id#

#define sl_btmesh_cmd_sar_config_client_deinit_id
Value:
0x02620028

sl_btmesh_cmd_sar_config_client_get_sar_transmitter_id#

#define sl_btmesh_cmd_sar_config_client_get_sar_transmitter_id
Value:
0x03620028

sl_btmesh_cmd_sar_config_client_set_sar_transmitter_id#

#define sl_btmesh_cmd_sar_config_client_set_sar_transmitter_id
Value:
0x04620028

sl_btmesh_cmd_sar_config_client_get_sar_receiver_id#

#define sl_btmesh_cmd_sar_config_client_get_sar_receiver_id
Value:
0x05620028

sl_btmesh_cmd_sar_config_client_set_sar_receiver_id#

#define sl_btmesh_cmd_sar_config_client_set_sar_receiver_id
Value:
0x06620028

sl_btmesh_rsp_sar_config_client_init_id#

#define sl_btmesh_rsp_sar_config_client_init_id
Value:
0x01620028

sl_btmesh_rsp_sar_config_client_deinit_id#

#define sl_btmesh_rsp_sar_config_client_deinit_id
Value:
0x02620028

sl_btmesh_rsp_sar_config_client_get_sar_transmitter_id#

#define sl_btmesh_rsp_sar_config_client_get_sar_transmitter_id
Value:
0x03620028

sl_btmesh_rsp_sar_config_client_set_sar_transmitter_id#

#define sl_btmesh_rsp_sar_config_client_set_sar_transmitter_id
Value:
0x04620028

sl_btmesh_rsp_sar_config_client_get_sar_receiver_id#

#define sl_btmesh_rsp_sar_config_client_get_sar_receiver_id
Value:
0x05620028

sl_btmesh_rsp_sar_config_client_set_sar_receiver_id#

#define sl_btmesh_rsp_sar_config_client_set_sar_receiver_id
Value:
0x06620028