Btmesh_firmware_update_server_api#
BT Mesh Firmware Update Server user-overridable API
Enumerations#
Verification step results.
Metadata check step result.
Definitions taken from BT Mesh Specification v1.1.
Typedefs#
Verification step results.
Metadata check step result.
Definitions taken from BT Mesh Specification v1.1.
Functions#
Enumeration Documentation#
sl_btmesh_fw_update_server_verify_state_e#
sl_btmesh_fw_update_server_verify_state_e
Verification step results.
| Enumerator | |
|---|---|
| BTMESH_FW_UPDATE_SERVER_VERIFY_PENDING | Verification pending.  | 
| BTMESH_FW_UPDATE_SERVER_VERIFY_ERROR | Verification error.  | 
| BTMESH_FW_UPDATE_SERVER_VERIFY_SUCCESS | Verification successful.  | 
sl_btmesh_fw_update_server_metadata_check_state_e#
sl_btmesh_fw_update_server_metadata_check_state_e
Metadata check step result.
| Enumerator | |
|---|---|
| BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_PENDING | Metadata check pending.  | 
| BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_ERROR | Metadata check error.  | 
| BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_SUCCESS | Metadata check successful.  | 
sl_btmesh_fw_update_server_additional_information_e#
sl_btmesh_fw_update_server_additional_information_e
Definitions taken from BT Mesh Specification v1.1.
| Enumerator | |
|---|---|
| BTMESH_FW_UPDATE_SERVER_ADDITIONAL_INFORMATION_NO_CHANGE | No changes to node composition data.  | 
| BTMESH_FW_UPDATE_SERVER_ADDITIONAL_INFORMATION_COMP_DATA_CHANGE_NO_REMOTE_PROV | Node composition data changed. The node does not support remote provisioning.  | 
| BTMESH_FW_UPDATE_SERVER_ADDITIONAL_INFORMATION_COMP_DATA_CHANGE_REMOTE_PROV | Node composition data changed, and remote provisioning is supported. The node supports remote provisioning and composition data page 0x80. Page 0x80 contains different composition data than page 0x0.  | 
| BTMESH_FW_UPDATE_SERVER_ADDITIONAL_INFORMATION_UNPROVISION | Node unprovisioned. The node is unprovisioned after successful application of a verified firmware image.  | 
| BTMESH_FW_UPDATE_SERVER_ADDITIONAL_INFORMATION_RESERVED_START | Start of reserved values.  | 
Typedef Documentation#
sl_btmesh_fw_update_server_verify_state_t#
typedef enum sl_btmesh_fw_update_server_verify_state_e sl_btmesh_fw_update_server_verify_state_t
Verification step results.
sl_btmesh_fw_update_server_metadata_check_state_t#
typedef enum sl_btmesh_fw_update_server_metadata_check_state_e sl_btmesh_fw_update_server_metadata_check_state_t
Metadata check step result.
sl_btmesh_fw_update_server_additional_information_t#
typedef enum sl_btmesh_fw_update_server_additional_information_e sl_btmesh_fw_update_server_additional_information_t
Definitions taken from BT Mesh Specification v1.1.
Function Documentation#
sl_btmesh_fw_update_server_verify_start#
sl_btmesh_fw_update_server_verify_state_t sl_btmesh_fw_update_server_verify_start (sl_bt_uuid_64_t const *const blob_id, uint8_t **const verify_chunk_buffer, uint32_t *const verify_chunk_size, const uint32_t blob_size)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_uuid_64_t const *const | [in] | blob_id | Identifier of the BLOB to be verified  | 
| uint8_t **const | [out] | verify_chunk_buffer | Verification buffer. User needs to pass the verification buffer to the framework. User also needs to free memory if it was allocated on heap, which could be done in sl_btmesh_fw_update_server_apply. If it's set to NULL, then no data is read from storage automatically during verification.  | 
| uint32_t *const | [out] | verify_chunk_size | Size of verification chunk. Progress calculation is based on this value.  | 
| const uint32_t | [in] | blob_size | Size of the BLOB to be verified  | 
User callback for determining the maximum chunk size of verification
Used to determine how big chunks can be for sl_btmesh_fw_update_server_verify_step
Returns
Current state of verification
Return values
BTMESH_FW_UPDATE_SERVER_VERIFY_PENDING: If further processing required
BTMESH_FW_UPDATE_SERVER_VERIFY_ERROR: In case of an error
BTMESH_FW_UPDATE_SERVER_VERIFY_SUCCESS: In case verification is done and successful
sl_btmesh_fw_update_server_verify_step#
sl_btmesh_fw_update_server_verify_state_t sl_btmesh_fw_update_server_verify_step (void const * data, const uint32_t len)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void const * | [in] | data | Buffered data  | 
| const uint32_t | [in] | len | Length of the buffer  | 
User callback to execute one step of the verification
Receives a chunk of data equal to or less in size defined with sl_btmesh_fw_update_server_verify_start
Returns
Current state of verification
Return values
BTMESH_FW_UPDATE_SERVER_VERIFY_PENDING: If further processing required
BTMESH_FW_UPDATE_SERVER_VERIFY_ERROR: In case of an error
BTMESH_FW_UPDATE_SERVER_VERIFY_SUCCESS: In case verification is done and successful
sl_btmesh_fw_update_server_verify_progress_ui_update#
void sl_btmesh_fw_update_server_verify_progress_ui_update (sl_btmesh_fw_update_server_verify_state_t status, uint32_t progress, uint32_t size)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_btmesh_fw_update_server_verify_state_t | [in] | status | Verification status  | 
| uint32_t | [in] | progress | Number of verified bytes  | 
| uint32_t | [in] | size | Total number of bytes which shall be verified  | 
User callback to update the user interface with verification progress
If FW_UPDATE_SERVER_VERIFY_PROGRESS_UI_UPDATE_PERIOD is not zero then it specifies the period of this function call in order to limit the user interface update rate. If the macro is zero then this function is called whenever verification is active and progress is made. 
sl_btmesh_fw_update_server_metadata_check_start#
sl_btmesh_fw_update_server_metadata_check_state_t sl_btmesh_fw_update_server_metadata_check_start (void const * metadata, const uint8_t len, sl_btmesh_fw_update_server_additional_information_t *const additional_information)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void const * | [in] | metadata | Buffered metadata  | 
| const uint8_t | [in] | len | Metadata length  | 
| sl_btmesh_fw_update_server_additional_information_t *const | [out] | additional_information | Used in BT Mesh response to metadata check  | 
User callback indicating start of metadata check
Returns
Current state of metadata check
Return values
BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_PENDING: If further processing required
BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_ERROR: In case of an error
BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_SUCCESS: In case metadata check is done and successful
sl_btmesh_firmware_update_server_metadata_check_step#
sl_btmesh_fw_update_server_metadata_check_state_t sl_btmesh_firmware_update_server_metadata_check_step (sl_btmesh_fw_update_server_additional_information_t * additional_information)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_btmesh_fw_update_server_additional_information_t * | [out] | additional_information | Used in BT Mesh response to metadata check  | 
User callback executing one step of metadata check
Returns
Current state of metadata check
Return values
BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_PENDING: If further processing required
BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_ERROR: In case of an error
BTMESH_FW_UPDATE_SERVER_METADATA_CHECK_SUCCESS: In case metadata check is done and successful
sl_btmesh_fw_update_server_update_start#
void sl_btmesh_fw_update_server_update_start (sl_bt_uuid_64_t const *const blob_id)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_uuid_64_t const *const | [in] | blob_id | Identifier of the BLOB containing firmware  | 
User callback indicating update start
Called after metadata check is done.
Can be redefined to accommodate user application functionality.
sl_btmesh_fw_update_server_update_canceled#
void sl_btmesh_fw_update_server_update_canceled (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
User callback indicating update cancellation
Can be redefined to accommodate user application functionality.
sl_btmesh_fw_update_server_update_aborted#
void sl_btmesh_fw_update_server_update_aborted (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
User callback indicating update abort
Can be redefined to accommodate user application functionality.
sl_btmesh_fw_update_server_apply#
void sl_btmesh_fw_update_server_apply (void )
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
User callback indicating firmware apply request
Can be redefined to accommodate user application functionality.
mesh_platform_get_installed_firmware_information#
sl_status_t mesh_platform_get_installed_firmware_information (uint8_t index, uint8_t * fwid_len, const uint8_t ** fwid_ptr, uint8_t * uri_len, const uint8_t ** uri_ptr)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | index | DFU Storage index  | 
| uint8_t * | [out] | fwid_len | Length of the firmware ID  | 
| const uint8_t ** | [out] | fwid_ptr | Pointer to the firmware ID  | 
| uint8_t * | [out] | uri_len | Length of the Uniform Resource Identifier (URI)  | 
| const uint8_t ** | [out] | uri_ptr | Pointer to the Uniform Resource Identifier (URI)  | 
Used to retrieve information about firmware stored on the device for DFU Returns
SL_STATUS_OK if successful, SL_STATUS_BT_MESH_DOES_NOT_EXIST if the index is invalid