You are viewing documentation for version:
PDFData structure of the upload_complete event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_upload_complete_s::elem_index
Server model element index
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_upload_complete_s::client_address
Address of the Distribution Client
size#
uint32_t sl_btmesh_evt_fw_dist_server_upload_complete_s::size
Upload size
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_fw_dist_server_upload_complete_s::blob_id
BLOB ID
fwid#
uint8array sl_btmesh_evt_fw_dist_server_upload_complete_s::fwid
FWID of the firmware image