You are viewing documentation for version:
PDFOOB Capabilities#
OOB capability bitmask constants
Macro Definition Documentation#
SL_BTMESH_PROV_OOB_OTHER#
#define SL_BTMESH_PROV_OOB_OTHER
Value:0x1
Uncategorized
SL_BTMESH_PROV_OOB_URI#
#define SL_BTMESH_PROV_OOB_URI
Value:0x2
URI or other electronic
SL_BTMESH_PROV_OOB_2D_MR_CODE#
#define SL_BTMESH_PROV_OOB_2D_MR_CODE
Value:0x4
2D machine-readable code
SL_BTMESH_PROV_OOB_BAR_CODE#
#define SL_BTMESH_PROV_OOB_BAR_CODE
Value:0x8
Barcode
SL_BTMESH_PROV_OOB_NFC#
#define SL_BTMESH_PROV_OOB_NFC
Value:0x10
NFC
SL_BTMESH_PROV_OOB_NUMBER#
#define SL_BTMESH_PROV_OOB_NUMBER
Value:0x20
Number
SL_BTMESH_PROV_OOB_STRING#
#define SL_BTMESH_PROV_OOB_STRING
Value:0x40
String
SL_BTMESH_PROV_OOB_RFU_7#
#define SL_BTMESH_PROV_OOB_RFU_7
Value:0x80
Reserved
SL_BTMESH_PROV_OOB_RFU_8#
#define SL_BTMESH_PROV_OOB_RFU_8
Value:0x100
Reserved
SL_BTMESH_PROV_OOB_RFU_9#
#define SL_BTMESH_PROV_OOB_RFU_9
Value:0x200
Reserved
SL_BTMESH_PROV_OOB_RFU_A#
#define SL_BTMESH_PROV_OOB_RFU_A
Value:0x400
Reserved
SL_BTMESH_PROV_OOB_LOC_ON_BOX#
#define SL_BTMESH_PROV_OOB_LOC_ON_BOX
Value:0x800
On the box
SL_BTMESH_PROV_OOB_LOC_IN_BOX#
#define SL_BTMESH_PROV_OOB_LOC_IN_BOX
Value:0x1000
Inside the box
SL_BTMESH_PROV_OOB_LOC_PAPER#
#define SL_BTMESH_PROV_OOB_LOC_PAPER
Value:0x2000
On a piece of paper
SL_BTMESH_PROV_OOB_LOC_MANUAL#
#define SL_BTMESH_PROV_OOB_LOC_MANUAL
Value:0x4000
In the device manual
SL_BTMESH_PROV_OOB_LOC_DEVICE#
#define SL_BTMESH_PROV_OOB_LOC_DEVICE
Value:0x8000
On the device
SL_BTMESH_PROV_OOB_RFU_MASK#
#define SL_BTMESH_PROV_OOB_RFU_MASK
Value:0x780
Mask of reserved bits