Scene Server#
Used to support the control and reporting functionality of a node that can participate in a scene. This component is prepared for integration into SOC applications. This is a No-Code component, if it is used with other compatible software components (eg.: CTL server).
Functions#
sl_status_t
sl_btmesh_scenes_init(void)
void
sl_btmesh_scene_server_on_event(sl_btmesh_msg_t *evt)
Function Documentation#
sl_btmesh_scenes_init#
sl_status_t sl_btmesh_scenes_init (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Scenes initialization. This should be called at each boot if provisioning is already done. Otherwise this function should be called after provisioning is completed. This function is called automatically after enabling the component.
Returns
Status of the initialization operation. Returns SL_STATUS_OK (0) if successful. Error code otherwise.
sl_btmesh_scene_server_on_event#
void sl_btmesh_scene_server_on_event (sl_btmesh_msg_t * evt)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_msg_t * | [in] | evt | Pointer to incoming scene server event. |
Handling of mesh scene events.
This function is called automatically after enabling the component.