Time Server#
Used to support the control and reporting functionality of a node that tracks time. This component is prepared for integration into SOC applications. This is a No-Code component.
Functions#
Function Documentation#
sl_btmesh_scenes_init#
sl_status_t sl_btmesh_scenes_init (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Scenes initialization. This should be called at each boot if provisioning is already done. Otherwise this function should be called after provisioning is completed. This function is called automatically after enabling the component.
Returns
Status of the initialization operation. Returns SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_time_server_on_event#
void sl_btmesh_time_server_on_event (sl_btmesh_msg_t * evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_msg_t * | [in] | evt | Pointer to incoming time event. |
Handling of mesh time events. It handles:
time_server_time_updated
time_server_time_zone_offset_updated
time_server_tai_utc_delta_updated
time_server_time_role_updated
This function is called automatically after enabling the component.