Mesh_blob_transfer_server_api#
BT Mesh BLOB Transfer Server user-overridable API
Functions#
void
sl_btmesh_blob_transfer_server_transfer_start(sl_bt_uuid_64_t const *const blob_id)
void
sl_btmesh_blob_transfer_server_transfer_progress(sl_bt_uuid_64_t const *const blob_id, float progress)
void
sl_btmesh_blob_transfer_server_transfer_done(sl_bt_uuid_64_t const *const blob_id)
void
sl_btmesh_blob_transfer_server_transfer_abort(sl_bt_uuid_64_t const *const blob_id)
Function Documentation#
sl_btmesh_blob_transfer_server_transfer_start#
void sl_btmesh_blob_transfer_server_transfer_start (sl_bt_uuid_64_t const *const blob_id)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const *const | [in] | blob_id | Identifier of BLOB to be transferred |
Called when starting BLOB transfer
sl_btmesh_blob_transfer_server_transfer_progress#
void sl_btmesh_blob_transfer_server_transfer_progress (sl_bt_uuid_64_t const *const blob_id, float progress)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const *const | [in] | blob_id | Identifier of the BLOB being transferred |
| float | [in] | progress | Progress in floating point percentage |
Called when new block is started
Note
Progress is incremented on a chunk basis, but user callback is called on block basis to avoid too frequent calls.
sl_btmesh_blob_transfer_server_transfer_done#
void sl_btmesh_blob_transfer_server_transfer_done (sl_bt_uuid_64_t const *const blob_id)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const *const | [in] | blob_id | Identifier of BLOB transferred |
Called when BLOB transfer is done
sl_btmesh_blob_transfer_server_transfer_abort#
void sl_btmesh_blob_transfer_server_transfer_abort (sl_bt_uuid_64_t const *const blob_id)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_bt_uuid_64_t const *const | [in] | blob_id | Identifier of BLOB being transferred |
Called when BLOB transfer is aborted
sl_btmesh_blob_transfer_server_storage_full#
void sl_btmesh_blob_transfer_server_storage_full (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Called when BLOB storage signals it's full