BLOB Transfer Client#
Provides BT Mesh BLOB (binary large object) Transfer Client functionality, defined in mesh specification. The BLOB Transfer Client model is used by a higher-layer application to transfer a BLOB to one or more BLOB Transfer Servers. The higher-layer application provides the inputs to the procedures executed by the client. This component is prepared for integration into SOC applications.
Modules#
sl_btmesh_blob_transfer_client_progress_t
sl_btmesh_blob_transfer_client_server_failed_t
sl_btmesh_blob_transfer_client_notification_t
Typedefs#
Callback function type for BLOB transfer client notifications.
Functions#
BLOB Transfer Client Kind.
BLOB Transfer Client Result.
Macros#
Invalid value for the binary logarithm of the block size.
Typedef Documentation#
sl_btmesh_blob_transfer_client_notify_cb_t#
sl_btmesh_blob_transfer_client_notify_cb_t )(const sl_btmesh_blob_transfer_client_notification_t *const notification)
Callback function type for BLOB transfer client notifications.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | notification | Pointer to the notification structure containing details about the event or update. |
This callback is invoked to notify the application about events or updates related to the BLOB transfer client. The notification details are provided through the sl_btmesh_blob_transfer_client_notification_t structure.
Function Documentation#
SL_ENUM#
SL_ENUM (sl_btmesh_blob_transfer_client_notification_kind_t )
BLOB Transfer Client Kind.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_blob_transfer_client_notification_kind_t | N/A |
SL_ENUM#
SL_ENUM (sl_btmesh_blob_transfer_client_result_t )
BLOB Transfer Client Result.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_blob_transfer_client_result_t | N/A |
sl_btmesh_blob_transfer_client_setup#
sl_status_t sl_btmesh_blob_transfer_client_setup (uint16_t elem_index, sl_bt_uuid_64_t blob_id, uint32_t blob_size, uint16_t appkey_index, uint8_t ttl, uint16_t timeout_base, uint16_t group_address, uuid_128 virtual_address, uint16_t multicast_threshold, size_t servers_len, const uint8_t * servers)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | The client model element index. |
| sl_bt_uuid_64_t | [in] | blob_id | The ID of the BLOB. |
| uint32_t | [in] | blob_size | The size of the BLOB. |
| uint16_t | [in] | appkey_index | Index of the application key to be used for communicating with the servers |
| uint8_t | [in] | ttl | The TTL to use when communicating with the servers. |
| uint16_t | [in] | timeout_base | If a Server does not respond within this time frame, it will be marked as inactive. |
| uint16_t | [in] | group_address | The group address to used if the |
| uuid_128 | [in] | virtual_address | Virtual address in case virtual addresses are used |
| uint16_t | [in] | multicast_threshold | If the number of servers for any step exceeds this number, the group address will be used. Otherwise, servers will be looped through one by one. |
| size_t | [in] | servers_len | Length of data in servers |
| const uint8_t * | [in] | servers | List of MBT server addresses, represented as little endian two byte sequences. |
Set up a new BLOB transfer.
Note
This shall not be called when the Distribution Server initiates the BLOB transfer because BT Mesh stack sets up the BLOB transfer inside the BT Mesh stack automatically.
Returns
Result of the BLOB Transfer setup
Return values
SL_STATUS_OK: if successful. Error code otherwise.
SL_STATUS_INVALID_STATE: if not Idle
sl_btmesh_blob_transfer_client_setup_data_provider_array#
sl_status_t sl_btmesh_blob_transfer_client_setup_data_provider_array (uint16_t elem_index, const uint8_t * array, uint32_t length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
| const uint8_t * | [in] | array | Pointer to an array which stores the BLOB data |
| uint32_t | [in] | length | Length of the array |
Set up an array data provider for a new BLOB transfer.
The BLOB transfer client reads the BLOB data from this array during chunk transfer.
Returns
Result of the Data Provider setup
Return values
SL_STATUS_OK: if successful
SL_STATUS_INVALID_STATE: Data Provider setup called in non-idle state
SL_STATUS_INVALID_PARAMETER: BLOB size inconsistency between the
sl_btmesh_blob_transfer_client_setup_data_provider_blob_storage#
sl_status_t sl_btmesh_blob_transfer_client_setup_data_provider_blob_storage (uint16_t elem_index, const sl_bt_uuid_64_t * blob_id)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
| const sl_bt_uuid_64_t * | [in] | blob_id | Pointer to the BLOB id |
Set up a BLOB storage data provider for a new BLOB transfer.
The BLOB Transfer Client reads the BLOB data from the BLOB storage based on the passed BLOB id.
Note
The BLOB id used to identify the BLOB data in the BLOB storage (on the client side) is likely not the same as the BLOB id used during the BLOB transfer to the servers.
Returns
Result of the Data Provider setup
Return values
SL_STATUS_OK: if successful
SL_STATUS_INVALID_STATE: Data Provider setup called in non-idle state
SL_STATUS_NOT_FOUND: BLOB is not found in the BLOB storage
SL_STATUS_INVALID_PARAMETER: BLOB size inconsistency between the
sl_btmesh_blob_transfer_client_set_params#
sl_status_t sl_btmesh_blob_transfer_client_set_params (uint16_t elem_index, uint16_t separation_time_ms, uint16_t retry_time_local_ms, uint16_t retry_time_push_ms, uint16_t retry_time_pull_ms, uint16_t retry_max_local, uint16_t retry_threshold_remote)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
| uint16_t | [in] | separation_time_ms | Minimum separation time between two chunks in the same block, in milliseconds |
| uint16_t | [in] | retry_time_local_ms | Local retry time of message transmission requests during query info, transfer start, block start, block query, chunk transfer and transfer cancel procedures. Local retry time is used when the BT Mesh stack rejects sending BLOB Transfer messages due to a recoverable error, so BT Mesh stack API returns with recoverable error code, for example due to lack of memory. Local retry time shall be greater than zero. |
| uint16_t | [in] | retry_time_push_ms | Retry time of message transmissions during push transfer. The transfer start, block start, block query and transfer cancel procedures use this retry time during push transfer to send the procedure specific message again if at least one receiver haven't responded when retry timeout is reached. The query info procedure use this retry time value when the push transfer mode is selected explicitly by upper layer or both transfer modes (push & pull) are allowed by the upper layer. |
| uint16_t | [in] | retry_time_pull_ms | Retry time of message transmissions during pull transfer. The transfer start, block start, block query and transfer cancel procedures use this retry time during pull transfer to send the procedure specific message again if at least one receiver haven't responded when this retry timeout is reached.The query info procedure use this retry time when the pull transfer mode is selected explicitly by upper layer. |
| uint16_t | [in] | retry_max_local | Local max retries of message transmission requests during query info, transfer start, block start, block query chunk transfer and transfer cancel procedures. Max local retry is used when the BT Mesh stack rejects sending BLOB Transfer messages due to a recoverable error, so BT Mesh stack API returns with recoverable error code, for example due to lack of memory |
| uint16_t | [in] | retry_threshold_remote | Retry threshold of frequent message transmissions during query info, transfer start, block start, block query and transfer cancel procedures before infrequent message transmission is activated with doubled retry time. |
Set up additional parameters for new BLOB transfers
The separation and retry parameters are set for all future BLOB Transfers until the next reset (stored in RAM). On reset, the respective default separation and retry parameters are set based on the component configuration at component initialization time.
Note
This function is separated from sl_btmesh_blob_transfer_client_setup because the sl_btmesh_blob_transfer_client_setup shall not be called when Firmware Distribution Server initiates the BLOB transfer because BT Mesh stack sets up the BLOB transfer inside the BT Mesh stack automatically.
Returns
Result of the parameter setup
Return values
SL_STATUS_OK: if successful
SL_STATUS_INVALID_STATE: Parameter setup called in non-idle state
SL_STATUS_INVALID_PARAMETER: One or more parameters are invalid
sl_btmesh_blob_transfer_client_start#
sl_status_t sl_btmesh_blob_transfer_client_start (uint16_t elem_index, sl_btmesh_mbt_client_transfer_mode_t transfer_mode, sl_btmesh_blob_transfer_client_notify_cb_t notify)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
| sl_btmesh_mbt_client_transfer_mode_t | [in] | transfer_mode | Allowed transfer mode |
| sl_btmesh_blob_transfer_client_notify_cb_t | [in] | notify | Function pointer to a notification callback function which is called in the following cases:
It is valid to pass NULL as notify parameter. If the callback function is null then no notification is initiated. If |
Starts a previously set up BLOB Transfer.
Returns
SL_STATUS_OK if successful. Error code otherwise
Return values
SL_STATUS_INVALID_PARAMETER: Invalid transfer mode
SL_STATUS_INVALID_STATE: BLOB Transfer Client busy with another transfer
SL_STATUS_INVALID_CONFIGURATION: No data provider was specified
sl_btmesh_blob_transfer_client_cancel#
void sl_btmesh_blob_transfer_client_cancel (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
Cancels an ongoing BLOB Transfer.
sl_btmesh_blob_transfer_client_abort#
sl_status_t sl_btmesh_blob_transfer_client_abort (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
Aborts an ongoing BLOB Transfer.
Note
This function is not to be used when the MBT client is interfaced by a higher layer component (e.g. distribution server).
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_blob_transfer_client_on_aborted#
sl_status_t sl_btmesh_blob_transfer_client_on_aborted (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
Informs BLOB Transfer Client SDK component that the transfer in MBT Client model of BT Mesh stack was aborted.
Note
This function shall be used only when the MBT client is interfaced by a higher layer component (e.g. distribution server). The MBT Client model can be aborted by higher layer models in the BT Mesh stack which is not reported in MBT Client model events so it shall be reported by calling this API.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_blob_transfer_client_on_suspended#
sl_status_t sl_btmesh_blob_transfer_client_on_suspended (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
Informs BLOB Transfer Client SDK component that the transfer in MBT Client model of BT Mesh stack was suspended.
Note
This function shall be used only when the MBT client is interfaced by a higher layer component (e.g. distribution server). The MBT Client model can be suspended by higher layer models in the BT Mesh stack which is not reported in MBT Client model events so it shall be reported by calling this API.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_blob_transfer_client_on_resumed#
sl_status_t sl_btmesh_blob_transfer_client_on_resumed (uint16_t elem_index)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | elem_index | Client model element index |
Informs BLOB Transfer Client SDK component that the transfer in MBT Client model of BT Mesh stack was resumed.
Note
This function shall be used only when the MBT client is interfaced by a higher layer component (e.g. distribution server). The MBT Client model can be resumed by higher layer models in the BT Mesh stack which is not reported in MBT Client model events so it shall be reported by calling this API.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_blob_transfer_client_on_event#
void sl_btmesh_blob_transfer_client_on_event (const sl_btmesh_msg_t *const evt)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_btmesh_msg_t *const | [in] | evt | Pointer to incoming event. |
Handle BLOB Transfer Client events.
This function is called automatically after enabling the component.
sl_btmesh_blob_transfer_client_calculate_block_size_log#
uint8_t sl_btmesh_blob_transfer_client_calculate_block_size_log (uint32_t blob_size, uint8_t block_size_log_min, uint8_t block_size_log_max, uint16_t block_count_max, uint16_t max_chunk_size_min, uint16_t max_chunks_min)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | blob_size | Size of the BLOB |
| uint8_t | [in] | block_size_log_min | Min allowed binary logarithm of the block size |
| uint8_t | [in] | block_size_log_max | Max allowed binary logarithm of the block size |
| uint16_t | [in] | block_count_max | Max allowed number of blocks |
| uint16_t | [in] | max_chunk_size_min | Max allowed chunk size in the current transfer |
| uint16_t | [in] | max_chunks_min | Max allowed number of chunks per block in the current transfer |
Calculates the binary logarithm of the block size for the current BLOB transfer from the provided parameters which are the result of the Retrieve Capabilities procedure of the BLOB Transfer.
The parameters passed represent the aggregated capabilities of the BLOB transfer client and every BLOB transfer server which participates in the current transfer.
The default implementation calculates the greatest possible block size from the parameters. If another implementation is required then the strong symbol definition shall be provided for this function with the implementation in the application code.
Returns
Binary logarithm of the selected block size for the current transfer
Return values
SL_BTMESH_BLOB_TRANSFER_CLIENT_INVALID_BLOCK_SIZE_LOG: Invalid parameters
sl_btmesh_blob_transfer_client_calculate_chunk_size#
uint16_t sl_btmesh_blob_transfer_client_calculate_chunk_size (uint8_t block_size_log, uint16_t max_chunk_size_min, uint16_t max_chunks_min, uint16_t nw_pdu_size)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | block_size_log | The selected binary logarithm of the block size during previous phase of the BLOB transfer |
| uint16_t | [in] | max_chunk_size_min | Max allowed chunk size in the current transfer |
| uint16_t | [in] | max_chunks_min | Max allowed number of chunks per block in the current transfer |
| uint16_t | [in] | nw_pdu_size | Size of Network PDU. If the Silicon Labs BT Mesh over advertisement extension proprietary feature is turned on then it can be greater than 29 bytes. |
Calculates the chunk size for the next block in the current BLOB transfer from the previously selected binary logarithm of the block size and from the result of the Retrieve Capabilities procedure of the BLOB Transfer.
If the configurable preferred chunk size is supported by all BLOB Transfer Servers then the default chunk size calculation algorithm selects it as chunk size of the block otherwise the chunk size is set to the closest value which fills all segments of the chunk. If another implementation is required then the strong symbol definition shall be provided for this function with the implementation in the application code.
Returns
Chunk size for next block in the current BLOB transfer
sl_btmesh_blob_transfer_client_transfer_mode_to_string#
const char * sl_btmesh_blob_transfer_client_transfer_mode_to_string (sl_btmesh_mbt_client_transfer_mode_t transfer_mode)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_mbt_client_transfer_mode_t | [in] | transfer_mode | transfer mode |
Provides string representation of transfer mode
It is guaranteed that this function returns a valid string even in case of invalid transfer mode.
Note
The to_string functions are used for log calls only in this component. If the logging is disabled then the linker can eliminate these functions.
Returns
String representation of transfer mode
Return values
INVALID: if the transfer mode is invalid
sl_btmesh_blob_transfer_client_mbt_phase_to_string#
const char * sl_btmesh_blob_transfer_client_mbt_phase_to_string (sl_btmesh_mbt_server_phase_t mbt_phase)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_mbt_server_phase_t | [in] | mbt_phase | MBT phase |
Provides string representation of MBT phase
It is guaranteed that this function returns a valid string even in case of invalid MBT phase.
Note
The to_string functions are used for log calls only in this component. If the logging is disabled then the linker can eliminate these functions.
Returns
String representation of MBT phase
Return values
INVALID: if the MBT phase is invalid
sl_btmesh_blob_transfer_client_mbt_status_to_string#
const char * sl_btmesh_blob_transfer_client_mbt_status_to_string (sl_btmesh_mbt_server_status_t mbt_status)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_btmesh_mbt_server_status_t | [in] | mbt_status | MBT status |
Provides string representation of MBT status
It is guaranteed that this function returns a valid string even in case of invalid MBT status.
Note
The to_string functions are used for log calls only in this component. If the logging is disabled then the linker can eliminate these functions.
Returns
String representation of MBT status
Return values
INVALID: if the MBT status is invalid
sl_btmesh_blob_transfer_client_get_max_servers#
uint16_t sl_btmesh_blob_transfer_client_get_max_servers (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Provides the maximum number of MBT servers the client is configured to handle
Returns
Value of SL_BTMESH_BLOB_TRANSFER_CLIENT_MAX_SERVERS_CFG_VAL