BLOB Transfer Server Failed Notification.
Public Attribute Documentation#
server_address#
uint16_t sl_btmesh_blob_transfer_client_server_failed_t::server_address
Address of the BLOB Transfer Server.
timeout#
uint8_t sl_btmesh_blob_transfer_client_server_failed_t::timeout
If a BLOB Transfer Server doesn't respond until a specified time then the timeout is set to 1
error#
uint8_t sl_btmesh_blob_transfer_client_server_failed_t::error
The error is set only if the timeout is zero and a BLOB Transfer Server has responded with non-zero status code (error) in BLOB Transfer Status or BLOB Block Status message