Modules#

EmberCommandEntry

EmberCommandState

Command Interpreter Plugin#

Process commands coming from the serial port.

Interpret serial port commands. See command-interpreter2.c for source code.

See the following application usage example followed by a brief explanation.

// Usage: network form 22 0xAB12 -3 { 00 01 02 A3 A4 A5 A6 A7 }
void formCommand(void)
{
  uint8_t channel = emberUnsignedCommandArgument(0);
  uint16_t panId  = emberUnsignedCommandArgument(1);
  int8_t power   = emberSignedCommandArgument(2);
  uint8_t length;
  uint8_t *eui64  = emberStringCommandArgument(3, &length);
  ...
  ... call emberFormNetwork() etc
  ...
}

// The main command table.
EmberCommandEntry emberCommandTable[] = {
  emberCommandEntrySubMenu("network",  networkCommands, "Network form/join commands"),
  emberCommandEntryAction("status",    statusCommand,   "Prints application status),
  ...
  emberCommandEntryTerminator()
};

// The table of network commands.
EmberCommandEntry networkCommands[] = {
  emberCommandEntryAction("form", formCommand, "uvsh", "Form a network"),
  { "join",       joinCommand, "uvsh" },
  ...
  emberCommandEntryTerminator()
};

void main(void)
{
   emberCommandReaderInit();
   while(0) {
     ...
     // Process input and print prompt if it returns true.
     if (emberProcessCommandInput(serialPort)) {
        emberSerialPrintf(1, "%p>", PROMPT);
     }
     ...
   }
}
  1. Applications specify the commands that can be interpreted by defining the emberCommandTable array of type EmberCommandEntry. The table includes the following information for each command:

    1. The full command name.

    2. The application's function name that implements the command.

    3. An EmberCommandEntry::argumentTypes string specifies the number and types of arguments the command accepts.

    4. A description string explains the command.

  2. A default error handler emberCommandErrorHandler() is provided to deal with the incorrect command input. Applications may override it.

  3. The application calls emberCommandReaderInit() to initialize and emberProcessCommandInput() in its main loop.

  4. Within the application's command functions, use emberXXXCommandArgument() functions to retrieve command arguments.

The command interpreter does extensive processing and validation of the command input before calling the function that implements the command. It checks that the number, type, syntax, and range of all arguments is correct. It performs any conversions necessary, for example, converting integers and strings input in hexadecimal notation into the corresponding bytes so that no additional parsing is necessary within command functions. If an error occurs in the command input, emberCommandErrorHandler() is called instead of a command function.

The command interpreter allows inexact matches of command names. The input command may be either shorter or longer than the actual command. However, if more than one inexact match is found and there is no exact match, an error of type EMBER_CMD_ERR_NO_SUCH_COMMAND is generated. To disable this feature, define EMBER_REQUIRE_EXACT_COMMAND_NAME in the application configuration header.

Retrieve Arguments#

Use the following functions that process commands to retrieve arguments from the command interpreter. These functions pull out unsigned integers, signed integers, strings, and hexadecimal strings. Index 0 is the first command argument.

uint32_t
int32_t
uint8_t *
emberStringCommandArgument(int8_t argNum, uint8_t *length)
const char *
uint8_t
emberGetStringArgument(int8_t argNum, uint8_t *destination, uint8_t maxLength, bool leftPad)
bool
emberGetIpArgument(uint8_t index, uint8_t *target)
bool
emberGetIpPrefixArgument(uint8_t index, uint8_t *target)
void
emberGetExtendedPanIdArgument(int8_t index, uint8_t *extendedPanId)
#define
emberCopyKeyArgument (index, keyDataPointer)

A convenience macro for copying security key arguments to an EmberKeyData pointer.

#define
emberCopyEui64Argument (index, eui64)

A convenience macro for copying eui64 arguments to an EmberEUI64.

#define
emberGetKeyArgument (index, keyDataPointer)

A convenience macro for copying security key arguments to an EmberKeyData pointer.

#define
emberGetEui64Argument (index, eui64)

Copy the EUI64 argument to the given EmberEui64 destination reversing the bytes. EUI64's are stored little endian so reversing the bytes means they are big endian in the input command string.

Callbacks#

void
emberCommandErrorHandler(EmberCommandStatus status, EmberCommandEntry *command)

Command Table Settings#

#define

The maximum number of arguments a command can have. A nested command counts as an argument.

#define

The maximum number of arguments a command can have. A nested command counts as an argument.

#define
EMBER_CUSTOM_COMMAND_BUFFER_LENGTH (EMBER_COMMAND_BUFFER_LENGTH - 3)

The maximum message size for custom commands reserves three bytes for the length (1 bytes) and the custom command identifier (2 bytes).

#define

Indicate whether or not the command entry structure includes descriptions for the commands. This consumes additional CONST space, which is expensive on the XAP. By default, descriptions are not included.

Enumerations#

enum
EMBER_CMD_SUCCESS
EMBER_CMD_ERR_PORT_PROBLEM
EMBER_CMD_ERR_NO_SUCH_COMMAND
EMBER_CMD_ERR_WRONG_NUMBER_OF_ARGUMENTS
EMBER_CMD_ERR_ARGUMENT_OUT_OF_RANGE
EMBER_CMD_ERR_ARGUMENT_SYNTAX_ERROR
EMBER_CMD_ERR_STRING_TOO_LONG
EMBER_CMD_ERR_INVALID_ARGUMENT_TYPE
}

Command error states.

Typedefs#

typedef void(*
typedef void
EmberCommandErrorHandler(EmberCommandStatus status, EmberCommandEntry *command)

Type of error handlers; the command argument is currently always NULL.

Functions#

void
emberPrintCommandUsage(EmberCommandEntry *entry)
void

Initialize the command interpreter.

bool
emberProcessCommandString(const uint8_t *input, uint16_t sizeOrPort)

Process the given string as a command.

uint8_t
emberHexToInt(uint8_t ch)

Return the value of a hexadecimal digit ch (0 - 15). Returns a value > 15 if ch is not a hexadecimal digit.

bool
emberStringToIpAddress(const uint8_t *string, uint8_t stringLength, uint8_t *target)

Parse textual representations of IPv6 addresses as described in http://www.ietf.org/rfc/rfc4291.txt.

bool
emberStringToIpPrefix(const uint8_t *string, uint8_t stringLength, uint8_t *target)

Parse textual representations of IPv6 prefixes as described in http://www.ietf.org/rfc/rfc4291.txt.

void
emberInitializeCommandState(EmberCommandState *state)

Must be called to initialize a command state before passing it to emberRunCommandInterpreter().

bool
emberRunCommandInterpreter(bool commandIsBinary, EmberCommandState *state, EmberCommandEntry *commands, EmberCommandErrorHandler *errorHandler, const uint8_t *input, uint16_t sizeOrPort)

For use when additional different command streams are used.

Macros#

#define
MAX_TOKEN_COUNT (EMBER_MAX_COMMAND_ARGUMENTS + 1)
#define
emberCommandEntryAction (name, command, arguments, description)
#define
emberCommandEntrySubMenu (name, nestedCommands, description)
#define
emberCommand emberCommandEntryAction
#define
emberNestedCommand emberCommandEntrySubMenu
#define

Process the input coming in on the given serial port.

Retrieve Arguments Documentation#

emberCommandArgumentCount#

uint8_t emberCommandArgumentCount (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns the number of arguments for the current command.


emberUnsignedCommandArgument#

uint32_t emberUnsignedCommandArgument (uint8_t argNum)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/AargNum

Retrieves unsigned integer arguments.


emberSignedCommandArgument#

int32_t emberSignedCommandArgument (uint8_t argNum)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/AargNum

Retrieve signed integer arguments.


emberStringCommandArgument#

uint8_t * emberStringCommandArgument (int8_t argNum, uint8_t * length)
Parameters
TypeDirectionArgument NameDescription
int8_tN/AargNum
uint8_t *N/Alength

Retrieve quoted string or hexadecimal string arguments. Hexadecimal strings are already converted into binary. ASCII strings are null terminated. The null terminator is not included in the returned length argument. To retrieve the name of the command itself, use an argNum of -1. For example, to retrieve the first character of the command, uint8_t firstChar = emberStringCommandArgument(-1, NULL)[0]. If the command is nested, an index of -2, -3, and so on retrieves the higher level command names. Note that [-1] only returns the text entered. If an abbreviated command name is entered, only the text entered will be returned with [-1].


emberCommandName#

const char * emberCommandName (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

A convenience macro for copying security key arguments to an EmberKeyData pointer.


emberGetStringArgument#

uint8_t emberGetStringArgument (int8_t argNum, uint8_t * destination, uint8_t maxLength, bool leftPad)
Parameters
TypeDirectionArgument NameDescription
int8_tN/AargNum
uint8_t *N/Adestination
uint8_tN/AmaxLength
boolN/AleftPad

Copy the string argument to the given destination up to maxLength. If the argument length is not zero but less than maxLength and leftPad is true, leading zeroes are prepended to bring the total length of the target up to maxLength. If the argument is longer than the maxLength, it is truncated to maxLength. Returns the minimum of the argument length and maxLength. ASCII strings are null terminated but the null terminator is not included in the returned length.

This function is commonly used for reading in hexadecimal strings, such as EUI64 or key data and left padding them with zeros. See emberGetKeyArgument and emberGetEui64Argument for convenience macros for this purpose.


emberGetIpArgument#

bool emberGetIpArgument (uint8_t index, uint8_t * target)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex
uint8_t *N/Atarget

Parse and return, via target, an IP address at the provided index. Returns true if an IP address was successfully parsed Returns false otherwise.


emberGetIpPrefixArgument#

bool emberGetIpPrefixArgument (uint8_t index, uint8_t * target)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex
uint8_t *N/Atarget

Parse and return, via target, an IP prefix at the provided index. Returns true if an IP prefix was successfully parsed. Returns false otherwise.


emberGetExtendedPanIdArgument#

void emberGetExtendedPanIdArgument (int8_t index, uint8_t * extendedPanId)
Parameters
TypeDirectionArgument NameDescription
int8_tN/Aindex
uint8_t *N/AextendedPanId

Copy the extended PAN ID argument to the given destination, reversing the bytes. Extended PAN IDs are stored little endian so reversing the bytes means they are big endian in the input command string.


emberCopyKeyArgument#

#define emberCopyKeyArgument
Value:
(emberGetStringArgument((index), \
emberKeyContents((keyDataPointer)), \
EMBER_ENCRYPTION_KEY_SIZE, \
TRUE))

A convenience macro for copying security key arguments to an EmberKeyData pointer.


emberCopyEui64Argument#

#define emberCopyEui64Argument
Value:
(index, eui64)

A convenience macro for copying eui64 arguments to an EmberEUI64.


emberGetKeyArgument#

#define emberGetKeyArgument
Value:
(emberGetStringArgument((index), \
emberKeyContents((keyDataPointer)), \
EMBER_ENCRYPTION_KEY_SIZE, \
true))

A convenience macro for copying security key arguments to an EmberKeyData pointer.


emberGetEui64Argument#

#define emberGetEui64Argument
Value:
(index, eui64)

Copy the EUI64 argument to the given EmberEui64 destination reversing the bytes. EUI64's are stored little endian so reversing the bytes means they are big endian in the input command string.


Callbacks Documentation#

emberCommandErrorHandler#

void emberCommandErrorHandler (EmberCommandStatus status, EmberCommandEntry * command)
Parameters
TypeDirectionArgument NameDescription
EmberCommandStatusN/Astatus
EmberCommandEntry *N/Acommand

Command Table Settings Documentation#

EMBER_MAX_COMMAND_ARGUMENTS#

#define EMBER_MAX_COMMAND_ARGUMENTS
Value:
20

The maximum number of arguments a command can have. A nested command counts as an argument.


EMBER_COMMAND_BUFFER_LENGTH#

#define EMBER_COMMAND_BUFFER_LENGTH
Value:
200

The maximum number of arguments a command can have. A nested command counts as an argument.


EMBER_CUSTOM_COMMAND_BUFFER_LENGTH#

#define EMBER_CUSTOM_COMMAND_BUFFER_LENGTH
Value:
(EMBER_COMMAND_BUFFER_LENGTH - 3)

The maximum message size for custom commands reserves three bytes for the length (1 bytes) and the custom command identifier (2 bytes).


EMBER_COMMAND_INTEPRETER_HAS_DESCRIPTION_FIELD#

#define EMBER_COMMAND_INTEPRETER_HAS_DESCRIPTION_FIELD

Indicate whether or not the command entry structure includes descriptions for the commands. This consumes additional CONST space, which is expensive on the XAP. By default, descriptions are not included.


Enumeration Documentation#

EmberCommandStatus#

EmberCommandStatus

Command error states.

If you change this list, also change the strings that describe these errors in the array emberCommandErrorNames[] in command-interpreter2-error.c.

Enumerator
EMBER_CMD_SUCCESS
EMBER_CMD_ERR_PORT_PROBLEM
EMBER_CMD_ERR_NO_SUCH_COMMAND
EMBER_CMD_ERR_WRONG_NUMBER_OF_ARGUMENTS
EMBER_CMD_ERR_ARGUMENT_OUT_OF_RANGE
EMBER_CMD_ERR_ARGUMENT_SYNTAX_ERROR
EMBER_CMD_ERR_STRING_TOO_LONG
EMBER_CMD_ERR_INVALID_ARGUMENT_TYPE

Typedef Documentation#

CommandAction#

typedef void(* CommandAction) (void) )(void)

EmberCommandErrorHandler#

typedef void EmberCommandErrorHandler(EmberCommandStatus status, EmberCommandEntry *command) (EmberCommandStatus status, EmberCommandEntry *command)

Type of error handlers; the command argument is currently always NULL.


Variable Documentation#

emberCommandTable#

EmberCommandEntry emberCommandTable[]

Function Documentation#

emberPrintCommandUsage#

void emberPrintCommandUsage (EmberCommandEntry * entry)
Parameters
TypeDirectionArgument NameDescription
EmberCommandEntry *N/Aentry

emberPrintCommandUsageNotes#

void emberPrintCommandUsageNotes (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

emberPrintCommandTable#

void emberPrintCommandTable (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

emberCommandClearBuffer#

void emberCommandClearBuffer (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

emberCommandReaderInit#

void emberCommandReaderInit (void )

Initialize the command interpreter.

Parameters
TypeDirectionArgument NameDescription
voidN/A

emberProcessCommandString#

bool emberProcessCommandString (const uint8_t * input, uint16_t sizeOrPort)

Process the given string as a command.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *N/Ainput
uint16_tN/AsizeOrPort

emberHexToInt#

uint8_t emberHexToInt (uint8_t ch)

Return the value of a hexadecimal digit ch (0 - 15). Returns a value > 15 if ch is not a hexadecimal digit.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Ach

emberStringToIpAddress#

bool emberStringToIpAddress (const uint8_t * string, uint8_t stringLength, uint8_t * target)

Parse textual representations of IPv6 addresses as described in http://www.ietf.org/rfc/rfc4291.txt.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *N/Astring
uint8_tN/AstringLength
uint8_t *N/Atarget

emberStringToIpPrefix#

bool emberStringToIpPrefix (const uint8_t * string, uint8_t stringLength, uint8_t * target)

Parse textual representations of IPv6 prefixes as described in http://www.ietf.org/rfc/rfc4291.txt.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *N/Astring
uint8_tN/AstringLength
uint8_t *N/Atarget

emberInitializeCommandState#

void emberInitializeCommandState (EmberCommandState * state)

Must be called to initialize a command state before passing it to emberRunCommandInterpreter().

Parameters
TypeDirectionArgument NameDescription
EmberCommandState *N/Astate

emberRunCommandInterpreter#

bool emberRunCommandInterpreter (bool commandIsBinary, EmberCommandState * state, EmberCommandEntry * commands, EmberCommandErrorHandler * errorHandler, const uint8_t * input, uint16_t sizeOrPort)

For use when additional different command streams are used.

Parameters
TypeDirectionArgument NameDescription
boolN/AcommandIsBinary
EmberCommandState *N/Astate
EmberCommandEntry *N/Acommands
EmberCommandErrorHandler *N/AerrorHandler
const uint8_t *N/Ainput
uint16_tN/AsizeOrPort

emberCommandReaderSetDefaultBase#

void emberCommandReaderSetDefaultBase (uint8_t base)
Parameters
TypeDirectionArgument NameDescription
uint8_tN/Abase

Macro Definition Documentation#

MAX_TOKEN_COUNT#

#define MAX_TOKEN_COUNT
Value:
(EMBER_MAX_COMMAND_ARGUMENTS + 1)

emberCommandEntryAction#

#define emberCommandEntryAction
Value:
(name, command, arguments, description)

emberCommandEntrySubMenu#

#define emberCommandEntrySubMenu
Value:
(name, nestedCommands, description)

emberCommandEntryTerminator#

#define emberCommandEntryTerminator
Value:
()

emberCommand#

#define emberCommand
Value:
emberCommandEntryAction

emberNestedCommand#

#define emberNestedCommand
Value:
emberCommandEntrySubMenu

emberProcessCommandInput#

#define emberProcessCommandInput
Value:
(port)

Process the input coming in on the given serial port.

Returns

  • true if an end of line character was read. If the application uses a command line prompt, this indicates it is time to print the prompt.

    void emberProcessCommandInput(uint8_t port);