Definitions for manufacturing tokens.
CAUTION: This file is generated by gen_all.py which invokes gen_em3xx_token_mfg_h.py.
This file should not be included directly. It is accessed by the other token files.
Please see stack/config/token-stack.h and hal/micro/token.h for a full explanation of the tokens.
The tokens listed below are the manufacturing tokens. This token definitions file is included from the master definitions file: stack/config/token-stack.h Please see that file for more details.
The user application can include its own manufacturing tokens in a header file similar to this one. The macro ::APPLICATION_MFG_TOKEN_HEADER should be defined to equal the name of the header file in which application manufacturing tokens are defined.
The macro DEFINE_MFG_TOKEN() should be used when instantiating a manufacturing token. Refer to the list of *_LOCATION defines to see what memory is allocated and what memory is unused/available.
REMEMBER: By definition, manufacturing tokens exist at fixed addresses. Tokens should not overlap.
Here is a basic example of a manufacturing token header file:
#define CREATOR_MFG_EXAMPLE 0x4242
#ifdef DEFINETYPES
typedef uint8_t tokTypeMfgExample[8];
#endif
#ifdef DEFINETOKENS
#define MFG_EXAMPLE_LOCATION 0x0980
DEFINE_MFG_TOKEN(MFG_EXAMPLE,
tokTypeMfgExample,
MFG_EXAMPLE_LOCATION,
{0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF})
#endif
Since this file contains both the typedefs and the token defs, there are two #defines used to select which one is needed when this file is included. #define DEFINETYPES is used to select the type definitions and #define DEFINETOKENS is used to select the token definitions. Refer to token.h and token.c to see how these are used.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#define DEFINE_MFG_TOKEN(name, type, address, ...) \
TOKEN_NEXT_ADDRESS(name, (address)) \
TOKEN_MFG(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#ifndef TOKEN_NEXT_ADDRESS
#define TOKEN_NEXT_ADDRESS(region, address)
#endif
// MANUFACTURING DATA
// *the addresses of these tokens must not change*
// MANUFACTURING CREATORS
// The creator codes are here in one list instead of next to their token
// definitions so comparison of the codes is easier. The only requirement
// on these creator definitions is that they all must be unique. A favorite
// method for picking creator codes is to use two ASCII characters in order
// to make the codes more memorable. Also, the msb of Stack and Manufacturing
// token creator codes is always 1, while the msb of Application token creator
// codes is always 0. This distinction allows Application tokens
// to freely use the lower 15 bits for creator codes without the risk of
// duplicating a Stack or Manufacturing token creator code.
//--- Fixed Information Block ---
#define CREATOR_MFG_CHIP_DATA 0xC344 // msb+'C'+'D'
#define CREATOR_MFG_PART_DATA 0xF064 // msb+'p'+'d'
#define CREATOR_MFG_TESTER_DATA 0xF464 // msb+'t'+'d'
#define CREATOR_MFG_EMBER_EUI_64 0xE545 // msb+'e'+'E'
#define CREATOR_MFG_ANALOG_TRIM_NORMAL 0xF46E // msb+'t'+'n'
#define CREATOR_MFG_ANALOG_TRIM_BOOST 0xF442 // msb+'t'+'B'
#define CREATOR_MFG_ANALOG_TRIM_BOTH 0xF462 // msb+'t'+'b'
#define CREATOR_MFG_REG_TRIM 0xF274 // msb+'r'+'t'
#define CREATOR_MFG_1V8_REG_VOLTAGE 0xF276 // msb+'r'+'v'
#define CREATOR_MFG_VREF_VOLTAGE 0xF676 // msb+'v'+'v'
#define CREATOR_MFG_TEMP_CAL 0xF463 // msb+'t'+'c'
#define CREATOR_MFG_TEST_TEMP 0xF474 // msb+'t'+'t'
#define CREATOR_MFG_FIB_VERSION 0xFF09
#define CREATOR_MFG_FIB_CHECKSUM 0xE663 // msb+'f'+'c'
#define CREATOR_MFG_FIB_OBS 0xE66F // msb+'f'+'o'
//--- Customer Information Block ---
#define CREATOR_MFG_CIB_OBS 0xE36F // msb+'c'+'o'
#define CREATOR_MFG_CUSTOM_VERSION 0xC356
#define CREATOR_MFG_CUSTOM_EUI_64 0xE345
#define CREATOR_MFG_STRING 0xED73
#define CREATOR_MFG_BOARD_NAME 0xC24E // msb+'B'+'N' (Board Name)
#define CREATOR_MFG_MANUF_ID 0xC944 // msb+'I'+'D' (Id)
#define CREATOR_MFG_PHY_CONFIG 0xD043 // msb+'P'+'C' (Phy Config)
#define CREATOR_MFG_BOOTLOAD_AES_KEY 0xC24B // msb+'B'+'K' (Bootloader Key)
#define CREATOR_MFG_EZSP_STORAGE 0xCD53
#define CREATOR_MFG_ASH_CONFIG 0xC143 // msb+'A'+'C' (ASH Config)
#define CREATOR_MFG_CBKE_DATA 0xC342 // msb+'C'+'B' (CBke)
#define CREATOR_MFG_INSTALLATION_CODE 0xC943 // msb+'I'+'C' (Installation Code)
#define CREATOR_MFG_OSC24M_BIAS_TRIM 0xB254 // msb+'2'+'T' (2[4mHz] Trim)
#define CREATOR_MFG_SYNTH_FREQ_OFFSET 0xD346 // msb+'S'+'F' (Synth Freq)
#define CREATOR_MFG_OSC24M_SETTLE_DELAY 0xB253 // msb+'2'+'S' (2[4mHz] Settle)
#define CREATOR_MFG_SECURITY_CONFIG 0xD343 // msb+'S'+'C' (Security Config)
#define CREATOR_MFG_CCA_THRESHOLD 0xC343 // msb+'C'+'C' (Clear Channel)
#define CREATOR_MFG_SECURE_BOOTLOADER_KEY 0xD342 // msb+'S'+'B' (Secure Bootloader)
#define CREATOR_MFG_ETHERNET_ADDRESS 0xC554 // msb + 'E' + 'T'
#define CREATOR_MFG_CBKE_283K1_DATA 0xC345 // msb+'C'+'B' (CBke) 283k1 ECC (a.k.a. SE 1.2)
#define CREATOR_MFG_XO_TUNE 0xD854 // msb+'X'+'T' (XO TUNE Value)
#define CREATOR_MFG_THREAD_JOIN_KEY 0xCA4B // msb+'J'+'K' (Join Key)
#define CREATOR_MFG_EUI_64 0xB634
// The master defines indicating the version number these definitions work with.
#define CURRENT_MFG_TOKEN_VERSION 0x01FE //MSB is version, LSB is complement
#define VALID_MFG_TOKEN_VERSIONS { 0x01FE, 0x02FD }
#define CURRENT_MFG_CUSTOM_VERSION 0x01FE //MSB is version, LSB is complement
#ifdef DEFINETYPES
//--- Fixed Information Block ---
typedef uint8_t tokTypeMfgChipData[24];
typedef uint8_t tokTypeMfgPartData[6];
typedef uint8_t tokTypeMfgTesterData[6];
typedef uint8_t tokTypeMfgEmberEui64[8];
typedef struct {
uint16_t iffilterL;
uint16_t lna;
uint16_t ifamp;
uint16_t rxadcH;
uint16_t prescalar;
uint16_t phdet;
uint16_t vco;
uint16_t loopfilter;
uint16_t pa;
uint16_t iqmixer;
} tokTypeMfgAnalogueTrim;
typedef struct {
uint16_t iffilterH;
uint16_t biasmaster;
uint16_t moddac;
uint16_t auxadc;
uint16_t caladc;
} tokTypeMfgAnalogueTrimBoth;
typedef struct {
uint8_t regTrim1V2;
uint8_t regTrim1V8;
} tokTypeMfgRegTrim;
typedef uint16_t tokTypeMfgRegVoltage1V8;
typedef uint16_t tokTypeMfgAdcVrefVoltage;
typedef uint16_t tokTypeMfgTempCal;
typedef struct {
int8_t temp1;
int8_t temp2;
} tokTypeMfgTestTemp;
typedef uint16_t tokTypeMfgFibVersion;
typedef uint16_t tokTypeMfgFibChecksum;
typedef struct {
uint16_t ob2;
uint16_t ob3;
uint16_t ob0;
uint16_t ob1;
} tokTypeMfgFibObs;
//--- Customer Information Block ---
typedef struct {
uint16_t ob0;
uint16_t ob1;
uint16_t ob2;
uint16_t ob3;
uint16_t ob4;
uint16_t ob5;
uint16_t ob6;
uint16_t ob7;
} tokTypeMfgCibObs;
typedef uint16_t tokTypeMfgCustomVersion;
typedef uint8_t tokTypeMfgCustomEui64[8];
typedef uint8_t tokTypeMfgString[16];
typedef uint8_t tokTypeMfgBoardName[16];
typedef uint16_t tokTypeMfgManufId;
typedef uint16_t tokTypeMfgPhyConfig;
typedef uint8_t tokTypeMfgBootloadAesKey[16];
typedef uint8_t tokTypeMfgEzspStorage[8];
typedef uint16_t tokTypeMfgAshConfig;
// Smart Energy 1.0 (ECC 163k1 based crypto - 80-bit symmetric equivalent)
typedef struct {
uint8_t certificate[48];
uint8_t caPublicKey[22];
uint8_t privateKey[21];
// The bottom flag bit is 1 for uninitialized, 0 for initialized.
// The other flag bits should be set to 0 at initialization.
uint8_t flags;
} tokTypeMfgCbkeData;
typedef struct {
// The bottom flag bit is 1 for uninitialized, 0 for initialized.
// Bits 1 and 2 give the size of the value string:
// 0 = 6 bytes, 1 = 8 bytes, 2 = 12 bytes, 3 = 16 bytes.
// The other flag bits should be set to 0 at initialization.
// Special flags support. Due to a bug in the way some customers
// had programmed the flags field, we will also examine the upper
// bits 9 and 10 for the size field. Those bits are also reserved.
uint16_t flags;
uint8_t value[16];
uint16_t crc;
} tokTypeMfgInstallationCode;
typedef uint16_t tokTypeMfgOsc24mBiasTrim;
typedef uint16_t tokTypeMfgSynthFreqOffset;
typedef uint16_t tokTypeMfgOsc24mSettleDelay;
typedef uint16_t tokTypeMfgSecurityConfig;
typedef uint16_t tokTypeMfgCcaThreshold;
typedef struct {
uint8_t data[16]; // AES-128 key
} tokTypeMfgSecureBootloaderKey;
typedef struct {
uint8_t data[6];
} tokTypeMfgEthernetAddress;
// Smart Energy 1.2 (ECC 283k1 based crypto - 128-bit symmetric equivalent)
typedef struct {
uint8_t certificate[74];
uint8_t caPublicKey[37];
uint8_t privateKey[36];
// The bottom flag bit is 1 for uninitialized, 0 for initialized.
// The other flag bits should be set to 0 at initialization.
uint8_t flags;
} tokTypeMfgCbke283k1Data;
typedef uint16_t tokTypeMfgXoTune;
// Network join key with max length of 32 bytes
typedef struct {
uint8_t joinKey[32];
uint16_t joinKeyLength;
} tokTypeMfgThreadJoinKey;
typedef uint8_t tokTypeMfgEui64[8];
#endif //DEFINETYPES
#ifdef DEFINETOKENS
//The Manufacturing tokens need to be stored at well-defined locations.
//None of these addresses should ever change without extremely great care.
//All locations are OR'ed with FIB_BOTTOM to make a full 32bit address.
//--- Fixed Information Block ---
// FIB Bootloader 0x0000 //1918 bytes
#define MFG_CHIP_DATA_LOCATION 0x077E // 24 bytes
#define MFG_PART_DATA_LOCATION 0x0796 // 6 bytes
#define MFG_TESTER_DATA_LOCATION 0x079C // 6 bytes
#define MFG_EMBER_EUI_64_LOCATION 0x07A2 // 8 bytes
#define MFG_ANALOG_TRIM_NORMAL_LOCATION 0x07AA // 20 bytes
#define MFG_ANALOG_TRIM_BOOST_LOCATION 0x07BE // 20 bytes
#define MFG_ANALOG_TRIM_BOTH_LOCATION 0x07D2 // 10 bytes
#define MFG_REG_TRIM_LOCATION 0x07DC // 2 bytes
#define MFG_1V8_REG_VOLTAGE_LOCATION 0x07DE // 2 bytes
#define MFG_VREF_VOLTAGE_LOCATION 0x07E0 // 2 bytes
#define MFG_TEMP_CAL_LOCATION 0x07E2 // 2 bytes
#define MFG_TEST_TEMP_LOCATION 0x07E4 // 2 bytes
#define MFG_FIB_VERSION_LOCATION 0x07F4 // 2 bytes
#define MFG_FIB_CHECKSUM_LOCATION 0x07F6 // 2 bytes
#define MFG_FIB_OBS_LOCATION 0x07F8 // 8 bytes
//--- Customer Information Block ---
// The CIB is a 2KB block starting at 0x08040800.
#define MFG_CIB_OBS_LOCATION 0x0800 // 128 bytes
#define MFG_CUSTOM_VERSION_LOCATION 0x0810 // 2 bytes
#define MFG_CUSTOM_EUI_64_LOCATION 0x0812 // 8 bytes
#define MFG_STRING_LOCATION 0x081A // 16 bytes
#define MFG_BOARD_NAME_LOCATION 0x082A // 16 bytes
#define MFG_MANUF_ID_LOCATION 0x083A // 2 bytes
#define MFG_PHY_CONFIG_LOCATION 0x083C // 2 bytes
#define MFG_BOOTLOAD_AES_KEY_LOCATION 0x083E // 16 bytes
#define MFG_EZSP_STORAGE_LOCATION 0x084E // 8 bytes
#define MFG_ASH_CONFIG_LOCATION 0x0856 // 40 bytes
#define MFG_CBKE_DATA_LOCATION 0x087E // 92 bytes
#define MFG_INSTALLATION_CODE_LOCATION 0x08DA // 20 bytes
#define MFG_OSC24M_BIAS_TRIM_LOCATION 0x08EE // 2 bytes
#define MFG_SYNTH_FREQ_OFFSET_LOCATION 0x08F0 // 2 bytes
#define MFG_OSC24M_SETTLE_DELAY_LOCATION 0x08F2 // 2 bytes
#define MFG_SECURITY_CONFIG_LOCATION 0x08F4 // 2 bytes
#define MFG_CCA_THRESHOLD_LOCATION 0x08F6 // 2 bytes
#define MFG_SECURE_BOOTLOADER_KEY_LOCATION 0x08F8 // 16 bytes
#define MFG_ETHERNET_ADDRESS_LOCATION 0x0908 // 6 bytes
#define MFG_CBKE_283K1_DATA_LOCATION 0x090E // 148 bytes
#define MFG_XO_TUNE_LOCATION 0x09A2 // 2 bytes
#define MFG_THREAD_JOIN_KEY_LOCATION 0x09A4 // 34 bytes
//--- Virtual MFG Tokens ---
#define MFG_EUI_64_LOCATION 0xB634 // 8 bytes
// Define the size of indexed token array
#define MFG_ASH_CONFIG_ARRAY_SIZE 20
//--- Fixed Information Block ---
TOKEN_NEXT_ADDRESS(MFG_CHIP_DATA_ADDR, MFG_CHIP_DATA_LOCATION)
TOKEN_MFG(MFG_CHIP_DATA, CREATOR_MFG_CHIP_DATA,
0, 0, tokTypeMfgChipData, 1,
{ 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF })
TOKEN_NEXT_ADDRESS(MFG_PART_DATA_ADDR, MFG_PART_DATA_LOCATION)
TOKEN_MFG(MFG_PART_DATA, CREATOR_MFG_PART_DATA,
0, 0, tokTypeMfgPartData, 1,
{ 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF })
TOKEN_NEXT_ADDRESS(MFG_TESTER_DATA_ADDR, MFG_TESTER_DATA_LOCATION)
TOKEN_MFG(MFG_TESTER_DATA, CREATOR_MFG_TESTER_DATA,
0, 0, tokTypeMfgTesterData, 1,
{ 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF })
TOKEN_NEXT_ADDRESS(MFG_EMBER_EUI_64_ADDR, MFG_EMBER_EUI_64_LOCATION)
TOKEN_MFG(MFG_EMBER_EUI_64, CREATOR_MFG_EMBER_EUI_64,
0, 0, tokTypeMfgEmberEui64, 1,
{ 3, 0, 0, 0, 0, 0, 0, 3 })
TOKEN_NEXT_ADDRESS(MFG_ANALOG_TRIM_NORMAL_ADDR, MFG_ANALOG_TRIM_NORMAL_LOCATION)
TOKEN_MFG(MFG_ANALOG_TRIM_NORMAL, CREATOR_MFG_ANALOG_TRIM_NORMAL,
0, 0, tokTypeMfgAnalogueTrim, 1,
{ 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF })
TOKEN_NEXT_ADDRESS(MFG_ANALOG_TRIM_BOOST_ADDR, MFG_ANALOG_TRIM_BOOST_LOCATION)
TOKEN_MFG(MFG_ANALOG_TRIM_BOOST, CREATOR_MFG_ANALOG_TRIM_BOOST,
0, 0, tokTypeMfgAnalogueTrim, 1,
{ 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF })
TOKEN_NEXT_ADDRESS(MFG_ANALOG_TRIM_BOTH_ADDR, MFG_ANALOG_TRIM_BOTH_LOCATION)
TOKEN_MFG(MFG_ANALOG_TRIM_BOTH, CREATOR_MFG_ANALOG_TRIM_BOTH,
0, 0, tokTypeMfgAnalogueTrimBoth, 1,
{ 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF })
TOKEN_NEXT_ADDRESS(MFG_REG_TRIM_ADDR, MFG_REG_TRIM_LOCATION)
TOKEN_MFG(MFG_REG_TRIM, CREATOR_MFG_REG_TRIM,
0, 0, tokTypeMfgRegTrim, 1,
{ 0xFF, 0xFF })
TOKEN_NEXT_ADDRESS(MFG_1V8_REG_VOLTAGE_ADDR, MFG_1V8_REG_VOLTAGE_LOCATION)
TOKEN_MFG(MFG_1V8_REG_VOLTAGE, CREATOR_MFG_1V8_REG_VOLTAGE,
0, 0, tokTypeMfgRegVoltage1V8, 1,
0xFFFF)
TOKEN_NEXT_ADDRESS(MFG_VREF_VOLTAGE_ADDR, MFG_VREF_VOLTAGE_LOCATION)
TOKEN_MFG(MFG_VREF_VOLTAGE, CREATOR_MFG_VREF_VOLTAGE,
0, 0, tokTypeMfgAdcVrefVoltage, 1,
0xFFFF)
TOKEN_NEXT_ADDRESS(MFG_TEMP_CAL_ADDR, MFG_TEMP_CAL_LOCATION)
TOKEN_MFG(MFG_TEMP_CAL, CREATOR_MFG_TEMP_CAL,
0, 0, tokTypeMfgTempCal, 1,
0xFFFF)
TOKEN_NEXT_ADDRESS(MFG_TEST_TEMP_ADDR, MFG_TEST_TEMP_LOCATION)
TOKEN_MFG(MFG_TEST_TEMP, CREATOR_MFG_TEST_TEMP,
0, 0, tokTypeMfgTestTemp, 1,
{ 0xFF, 0xFF })
TOKEN_NEXT_ADDRESS(MFG_FIB_VERSION_ADDR, MFG_FIB_VERSION_LOCATION)
TOKEN_MFG(MFG_FIB_VERSION, CREATOR_MFG_FIB_VERSION,
0, 0, tokTypeMfgFibVersion, 1,
CURRENT_MFG_TOKEN_VERSION)
TOKEN_NEXT_ADDRESS(MFG_FIB_CHECKSUM_ADDR, MFG_FIB_CHECKSUM_LOCATION)
TOKEN_MFG(MFG_FIB_CHECKSUM, CREATOR_MFG_FIB_CHECKSUM,
0, 0, tokTypeMfgFibChecksum, 1,
0xFFFF)
TOKEN_NEXT_ADDRESS(MFG_FIB_OBS_ADDR, MFG_FIB_OBS_LOCATION)
TOKEN_MFG(MFG_FIB_OBS, CREATOR_MFG_FIB_OBS,
0, 0, tokTypeMfgFibObs, 1,
{ 0xFFFF, 0x03FC, 0xAA55, 0xFFFF })
//--- Customer Information Block ---
TOKEN_NEXT_ADDRESS(MFG_CIB_OBS_ADDR, MFG_CIB_OBS_LOCATION)
TOKEN_MFG(MFG_CIB_OBS, CREATOR_MFG_CIB_OBS,
0, 0, tokTypeMfgCibObs, 1,
{ 0x5AA5, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF })
TOKEN_NEXT_ADDRESS(MFG_CUSTOM_VERSION_ADDR, MFG_CUSTOM_VERSION_LOCATION)
TOKEN_MFG(MFG_CUSTOM_VERSION, CREATOR_MFG_CUSTOM_VERSION,
0, 0, tokTypeMfgCustomVersion, 1,
CURRENT_MFG_CUSTOM_VERSION)
TOKEN_NEXT_ADDRESS(MFG_CUSTOM_EUI_64_ADDR, MFG_CUSTOM_EUI_64_LOCATION)
TOKEN_MFG(MFG_CUSTOM_EUI_64, CREATOR_MFG_CUSTOM_EUI_64,
0, 0, tokTypeMfgCustomEui64, 1,
{ 0, 3, 3, 3, 3, 3, 3, 0 })
TOKEN_NEXT_ADDRESS(MFG_STRING_ADDR, MFG_STRING_LOCATION)
TOKEN_MFG(MFG_STRING, CREATOR_MFG_STRING,
0, 0, tokTypeMfgString, 1,
{ 0, })
TOKEN_NEXT_ADDRESS(MFG_BOARD_NAME_ADDR, MFG_BOARD_NAME_LOCATION)
TOKEN_MFG(MFG_BOARD_NAME, CREATOR_MFG_BOARD_NAME,
0, 0, tokTypeMfgBoardName, 1,
{ 0, })
TOKEN_NEXT_ADDRESS(MFG_MANUF_ID_ADDR, MFG_MANUF_ID_LOCATION)
TOKEN_MFG(MFG_MANUF_ID, CREATOR_MFG_MANUF_ID,
0, 0, tokTypeMfgManufId, 1,
{ 0x00, 0x00, }) // default to 0 for ember
TOKEN_NEXT_ADDRESS(MFG_PHY_CONFIG_ADDR, MFG_PHY_CONFIG_LOCATION)
TOKEN_MFG(MFG_PHY_CONFIG, CREATOR_MFG_PHY_CONFIG,
0, 0, tokTypeMfgPhyConfig, 1,
{ 0x00, 0x00, }) // default to non-boost mode, internal pa.
TOKEN_NEXT_ADDRESS(MFG_BOOTLOAD_AES_KEY_ADDR, MFG_BOOTLOAD_AES_KEY_LOCATION)
TOKEN_MFG(MFG_BOOTLOAD_AES_KEY, CREATOR_MFG_BOOTLOAD_AES_KEY,
0, 0, tokTypeMfgBootloadAesKey, 1,
{ 0xFF, }) // default key is all f's
TOKEN_NEXT_ADDRESS(MFG_EZSP_STORAGE_ADDR, MFG_EZSP_STORAGE_LOCATION)
TOKEN_MFG(MFG_EZSP_STORAGE, CREATOR_MFG_EZSP_STORAGE,
0, 0, tokTypeMfgEzspStorage, 1,
{ 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF })
TOKEN_NEXT_ADDRESS(MFG_ASH_CONFIG_ADDR, MFG_ASH_CONFIG_LOCATION)
TOKEN_MFG(MFG_ASH_CONFIG, CREATOR_MFG_ASH_CONFIG,
0, 1, tokTypeMfgAshConfig, MFG_ASH_CONFIG_ARRAY_SIZE,
{ 0xFFFF, })
TOKEN_NEXT_ADDRESS(MFG_CBKE_DATA_ADDR, MFG_CBKE_DATA_LOCATION)
TOKEN_MFG(MFG_CBKE_DATA, CREATOR_MFG_CBKE_DATA,
0, 0, tokTypeMfgCbkeData, 1,
{ 0xFF, })
TOKEN_NEXT_ADDRESS(MFG_INSTALLATION_CODE_ADDR, MFG_INSTALLATION_CODE_LOCATION)
TOKEN_MFG(MFG_INSTALLATION_CODE, CREATOR_MFG_INSTALLATION_CODE,
0, 0, tokTypeMfgInstallationCode, 1,
{ 0xFF, })
TOKEN_NEXT_ADDRESS(MFG_OSC24M_BIAS_TRIM_ADDR, MFG_OSC24M_BIAS_TRIM_LOCATION)
TOKEN_MFG(MFG_OSC24M_BIAS_TRIM, CREATOR_MFG_OSC24M_BIAS_TRIM,
0, 0, tokTypeMfgOsc24mBiasTrim, 1,
{ 0xFF, })
TOKEN_NEXT_ADDRESS(MFG_SYNTH_FREQ_OFFSET_ADDR, MFG_SYNTH_FREQ_OFFSET_LOCATION)
TOKEN_MFG(MFG_SYNTH_FREQ_OFFSET, CREATOR_MFG_SYNTH_FREQ_OFFSET,
0, 0, tokTypeMfgSynthFreqOffset, 1,
{ 0xFF, 0xFF, })
TOKEN_NEXT_ADDRESS(MFG_OSC24M_SETTLE_DELAY_ADDR, MFG_OSC24M_SETTLE_DELAY_LOCATION)
TOKEN_MFG(MFG_OSC24M_SETTLE_DELAY, CREATOR_MFG_OSC24M_SETTLE_DELAY,
0, 0, tokTypeMfgOsc24mSettleDelay, 1,
100)
TOKEN_NEXT_ADDRESS(MFG_SECURITY_CONFIG_ADDR, MFG_SECURITY_CONFIG_LOCATION)
TOKEN_MFG(MFG_SECURITY_CONFIG, CREATOR_MFG_SECURITY_CONFIG,
0, 0, tokTypeMfgSecurityConfig, 1,
{ 0xFF, 0xFF })
TOKEN_NEXT_ADDRESS(MFG_CCA_THRESHOLD_ADDR, MFG_CCA_THRESHOLD_LOCATION)
TOKEN_MFG(MFG_CCA_THRESHOLD, CREATOR_MFG_CCA_THRESHOLD,
0, 0, tokTypeMfgCcaThreshold, 1,
{ 0xFF, 0xFF, })
TOKEN_NEXT_ADDRESS(MFG_SECURE_BOOTLOADER_KEY_ADDR, MFG_SECURE_BOOTLOADER_KEY_LOCATION)
TOKEN_MFG(MFG_SECURE_BOOTLOADER_KEY, CREATOR_MFG_SECURE_BOOTLOADER_KEY,
0, 0, tokTypeMfgSecureBootloaderKey, 1,
{ 0xFF, }) // default key is all f's
TOKEN_NEXT_ADDRESS(MFG_ETHERNET_ADDRESS_ADDR, MFG_ETHERNET_ADDRESS_LOCATION)
TOKEN_MFG(MFG_ETHERNET_ADDRESS, CREATOR_MFG_ETHERNET_ADDRESS,
0, 0, tokTypeMfgEthernetAddress, 1,
{ 0xFF, }) // default address is unset (all F's)
TOKEN_NEXT_ADDRESS(MFG_CBKE_283K1_DATA_ADDR, MFG_CBKE_283K1_DATA_LOCATION)
TOKEN_MFG(MFG_CBKE_283K1_DATA, CREATOR_MFG_CBKE_283K1_DATA,
0, 0, tokTypeMfgCbke283k1Data, 1,
{ 0xFF, })
TOKEN_NEXT_ADDRESS(MFG_XO_TUNE_ADDR, MFG_XO_TUNE_LOCATION)
TOKEN_MFG(MFG_XO_TUNE, CREATOR_MFG_XO_TUNE,
0, 0, tokTypeMfgXoTune, 1,
{ 0xFFFF })
TOKEN_NEXT_ADDRESS(MFG_THREAD_JOIN_KEY_ADDR, MFG_THREAD_JOIN_KEY_LOCATION)
TOKEN_MFG(MFG_THREAD_JOIN_KEY, CREATOR_MFG_THREAD_JOIN_KEY,
0, 0, tokTypeMfgThreadJoinKey, 1,
{ 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFFFF })
TOKEN_NEXT_ADDRESS(MFG_EUI_64_ADDR, MFG_EUI_64_LOCATION)
TOKEN_MFG(MFG_EUI_64, CREATOR_MFG_EUI_64,
0, 0, tokTypeMfgEui64, 1,
{ 3, 3, 3, 3, 0, 0, 0, 0 })
#endif //DEFINETOKENS
#ifdef APPLICATION_MFG_TOKEN_HEADER
#include APPLICATION_MFG_TOKEN_HEADER
#endif
#undef TOKEN_NEXT_ADDRESS
Convenience Macros#
The following convenience macros are used to simplify the definition process for commonly specified parameters to the basic TOKEN_DEF macro. Please see hal/micro/token.h for a more complete explanation.
Macros#
Convenience Macros Documentation#
DEFINE_MFG_TOKEN#
#define DEFINE_MFG_TOKENValue: