Stack Information#

Connect API for accessing and modifying stack states and behaviors.

See stack-info.h for source code.

Modules#

Stack Counters

Handlers#

void
emberStackStatusHandler(EmberStatus status)

A callback invoked when the status of the stack changes.

void

This handler is invoked in ISR context when certain stack-related ISR routines fire.

bool
emberStackIdleHandler(uint32_t *idleTimeMs)

A callback to allow the application to manage idling the MCU.

void

The radio calibration callback function.

void
emberChildJoinHandler(EmberNodeType nodeType, EmberNodeId nodeId)

Invoked at coordinator, range extender, or mac mode nodes when a new child has joined the device.

APIs#

void

Immediately turns the radio power completely off.

void

Power up the radio. Typically called coming out of sleep.

Return the current join status.

bool

Indicate whether the stack is currently up.

emberSetSecurityKey(EmberKeyData *key)

Write a key at the address of the formerly used security key. The key set by this function will not be used by the stack. The API is meant to be used to erase a key as it is now managed by PSA Crypto API.

emberGetSecurityKey(EmberKeyData *key)

Get the legacy security key. This function does not return the value set with the PSA Crypto API.

emberSetRadioChannelExtended(uint16_t channel, bool persistent)

Set the channel for sending and receiving messages on the current network. The available channels depend on the radio config you use. Channels can differ more than the frequency if it's a multi-PHY config.

emberSetRadioChannel(uint16_t channel)

Set the channel for sending and receiving messages on the current network. The available channels depend on the radio config you use. Channels can differ more than the frequency if it's a multi-PHY config.

uint16_t

Get the radio channel, to which a node is set, on the current network. The available channels depend on the radio config you use. Channels can differ more than the frequency if it's a multi-PHY config.

uint16_t

Get the first available channel in the current radio configuration.

emberPhyConfigInit(EmberPhyType phyType)

Indicate if the PHY configuration of the stack. Currently only supporting EMBER_RADIO_CONFIGURATOR and EMBER_STANDARD_PHY_2_4GHZ. It must be called before initializing the stack.

emberCalibrateCurrentChannelExtended(uint32_t calValueIn, uint32_t *calValueOut)

Perform image rejection calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

Perform image rejection calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

emberApplyIrCalibration(uint32_t calValue)

Apply Image Rejection calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

Perform Temperature VCO calibration calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

Fetch calibration type associated to the latest emberRadioNeedsCalibratingHandler() callback.

emberSetRadioPower(int16_t power, bool persistent)

Set the radio output power at which a node is to operate for the current network. The radio has a finite power resolution, so it will approximate the requested power with the closest possible value at or below the requested value.

int16_t

Get the radio output power of the current network at which a node is operating. This might be different to what you set using emberSetRadioPower because the radio has a finite power resolution, and emberSetRadioPower must approximate to the closest possible value at or below the requested value. This API however returns with the actual setting.

Allow the application to turn the radio on/off. This API is intended for use with direct devices only.

Set if the stack should forward unencrypted messages to the application.

emberSetMacParams(int8_t ccaThreshold, uint8_t maxCcaAttempts, uint8_t minBackoffExp, uint8_t maxBackoffExp, uint16_t ccaBackoff, uint16_t ccaDuration, uint8_t maxRetries, uint32_t csmaTimeout, uint16_t ackTimeout)

Set the MAC layer transmission parameters.

emberMacGetParentAddress(EmberMacAddress *parentAddress)

Retrieve the parent address. This API can be invoked only for nodes of EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE type.

uint32_t
emberStackIdleTimeMs(uint16_t *currentStackTasks)

Return the time in milliseconds the stack could idle for.

uint32_t

Return the current time in milliseconds.

uint16_t

Return a bitmask indicating the stack's current tasks.

bool

Indicate whether the stack is currently in a state with no high-priority tasks and may sleep.

bool

Indicate whether the stack currently has any pending tasks.

uint8_t *

Return the EUI64 ID of the local node.

bool
emberIsLocalEui64(EmberEUI64 eui64)

Determine whether eui64 is the local node's EUI64 ID. EUI64 is easily accessible in SoC mode, but in Host-NCP, the address is stored on the NCP. This API can be used on the Host to compare a value with the locally stored one.

Return the 16-bit node ID of local node on the current network.

Return the local node's PAN ID of the current network.

Return an EmberNodeType value indicating the type of the node.

Return the parent's node ID.

emberGetVersionInfo(uint16_t *platform_version, uint16_t *connect_stack_version, uint32_t *bootloader_version)

Get the Platform, Stack and bootloader versions all at once. The version format are not all the same. Please refer to the corresponding documentation to handle the information correctly. The Platform version corresponds to the deprecated GSDK version.

Macros#

#define
EMBER_HIGH_PRIORITY_TASKS (EMBER_OUTGOING_MESSAGES | EMBER_INCOMING_MESSAGES | EMBER_RADIO_IS_ON)

A mask of the tasks that prevent a device from sleeping.

#define

Invalid channel number.

Handlers Documentation#

emberStackStatusHandler#

void emberStackStatusHandler (EmberStatus status)

A callback invoked when the status of the stack changes.

The application is free to begin messaging once it receives the EMBER_NETWORK_UP status.


Definition at line 72 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberStackIsrHandler#

void emberStackIsrHandler (void )

This handler is invoked in ISR context when certain stack-related ISR routines fire.

Parameters
N/A

Definition at line 77 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberStackIdleHandler#

bool emberStackIdleHandler (uint32_t * idleTimeMs)

A callback to allow the application to manage idling the MCU.

Parameters
[inout]idleTimeMs

A pointer to the time in millisecond the stack is allowed to idle. If the application decides to manage idling the MCU, it should update the passed value with the actual time the MCU was idled.

Returns

  • true if the application is managing idling the MCU, false otherwise. If this function returns false, the stack will manage idling the MCU.


Definition at line 88 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberRadioNeedsCalibratingHandler#

void emberRadioNeedsCalibratingHandler (void )

The radio calibration callback function.

Parameters
N/A

This handler is invoked by the stack upon receiving a "calibration needed" event from the radio to inform the application that it should perform calibration of the current channel as soon as possible using the emberCalibrateCurrentChannel() API. While calibration only takes tens of microseconds, the application can failsafe any critical processes or peripherals before calling emberCalibrateCurrentChannel(). The application must call emberCalibrateCurrentChannel() in response to this callback to maintain expected radio performance.


Definition at line 102 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberChildJoinHandler#

void emberChildJoinHandler (EmberNodeType nodeType, EmberNodeId nodeId)

Invoked at coordinator, range extender, or mac mode nodes when a new child has joined the device.

Parameters
[in]nodeType

The role of the joining device (EMBER_STAR_RANGE_EXTENDER, EMBER_STAR_END_DEVICE, EMBER_STAR_SLEEPY_END_DEVICE, EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE).

[in]nodeId

The node ID of the joining device.


Definition at line 615 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

APIs Documentation#

emberStackPowerDown#

void emberStackPowerDown (void )

Immediately turns the radio power completely off.

Parameters
N/A

After calling this function, do not call any other stack function except emberStackPowerUp() because all other stack functions require that the radio is powered to operate properly.


Definition at line 118 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberStackPowerUp#

void emberStackPowerUp (void )

Power up the radio. Typically called coming out of sleep.

Parameters
N/A

For non-sleepy devices, also turns the radio on and leaves it in RX mode.


Definition at line 124 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberNetworkState#

EmberNetworkStatus emberNetworkState (void )

Return the current join status.

Parameters
N/A

Returns a value indicating whether the node is joining, joined to, or leaving a network.

Returns


Definition at line 133 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberStackIsUp#

bool emberStackIsUp (void )

Indicate whether the stack is currently up.

Parameters
N/A

Returns true if the stack is joined to a network and ready to send and receive messages. This reflects only the state of the local node and does not indicate whether or not other nodes are able to communicate with this node.

Returns

  • true if the stack is up, false otherwise.


Definition at line 144 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberSetSecurityKey#

EmberStatus emberSetSecurityKey (EmberKeyData * key)

Write a key at the address of the formerly used security key. The key set by this function will not be used by the stack. The API is meant to be used to erase a key as it is now managed by PSA Crypto API.

Parameters
[in]key

An EmberKeyData value containing the security key to be set.

Returns


Definition at line 156 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetSecurityKey#

EmberStatus emberGetSecurityKey (EmberKeyData * key)

Get the legacy security key. This function does not return the value set with the PSA Crypto API.

Parameters
[in]key

An EmberKeyData where the legcay security key will be stored

Returns

  • An EmberStatus value of EMBER_SUCCESS if the key was successfully read.


Definition at line 166 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberSetRadioChannelExtended#

EmberStatus emberSetRadioChannelExtended (uint16_t channel, bool persistent)

Set the channel for sending and receiving messages on the current network. The available channels depend on the radio config you use. Channels can differ more than the frequency if it's a multi-PHY config.

Parameters
[in]channel

A desired radio channel.

[in]persistent

A flag to instruct the stack to save the channel setting in persistent or not. Each persistent call triggers a token write. Excessive usage might cause flash to wear-out.

Note

  • Care should be taken when using this API. All devices on a network must use the same channel.

Returns


Definition at line 222 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberSetRadioChannel#

EmberStatus emberSetRadioChannel (uint16_t channel)

Set the channel for sending and receiving messages on the current network. The available channels depend on the radio config you use. Channels can differ more than the frequency if it's a multi-PHY config.

Parameters
[in]channel

A desired radio channel.

Note

  • Care should be taken when using this API. All devices on a network must use the same channel. Each call triggers a token write. Excessive usage might cause flash to wear-out.

Returns


Definition at line 242 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetRadioChannel#

uint16_t emberGetRadioChannel (void )

Get the radio channel, to which a node is set, on the current network. The available channels depend on the radio config you use. Channels can differ more than the frequency if it's a multi-PHY config.

Parameters
N/A

Returns

  • The current radio channel.


Definition at line 250 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetDefaultChannel#

uint16_t emberGetDefaultChannel (void )

Get the first available channel in the current radio configuration.

Parameters
N/A

Returns

  • The first available channel in the radio configuration. 0xffff if error


Definition at line 257 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberPhyConfigInit#

EmberStatus emberPhyConfigInit (EmberPhyType phyType)

Indicate if the PHY configuration of the stack. Currently only supporting EMBER_RADIO_CONFIGURATOR and EMBER_STANDARD_PHY_2_4GHZ. It must be called before initializing the stack.

Parameters
N/AphyType

Returns


Definition at line 267 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberCalibrateCurrentChannelExtended#

EmberStatus emberCalibrateCurrentChannelExtended (uint32_t calValueIn, uint32_t * calValueOut)

Perform image rejection calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

Parameters
[in]calValueIn

the calibration value to use. Set to EMBER_CAL_INVALID_VALUE to perform automatic calibration.

[out]calValueOut

a pointer to the calibration value that was used. This parameter is ignored when set to NULL.

Returns

  • An EmberStatus value indicating the success or failure of the command.


Definition at line 286 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberCalibrateCurrentChannel#

EmberStatus emberCalibrateCurrentChannel (void )

Perform image rejection calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

Parameters
N/A

Definition at line 297 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberApplyIrCalibration#

EmberStatus emberApplyIrCalibration (uint32_t calValue)

Apply Image Rejection calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

Parameters
[in]calValue

the calibration value to apply. Should not be set to EMBER_CAL_INVALID_VALUE.

Returns

  • An EmberStatus value indicating the success or failure of the command.


Definition at line 313 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberTempCalibration#

EmberStatus emberTempCalibration (void )

Perform Temperature VCO calibration calibration on the current channel. The stack will notify the application that it needs channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Note if this function is called when the radio is off, it will turn the radio on and leave it on.

Parameters
N/A

Returns

  • An EmberStatus value indicating the success or failure of the command.


Definition at line 326 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetCalType#

EmberCalType emberGetCalType (void )

Fetch calibration type associated to the latest emberRadioNeedsCalibratingHandler() callback.

Parameters
N/A

Returns

  • An EmberCalType value indicating which type of calibration should be performed.


Definition at line 334 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberSetRadioPower#

EmberStatus emberSetRadioPower (int16_t power, bool persistent)

Set the radio output power at which a node is to operate for the current network. The radio has a finite power resolution, so it will approximate the requested power with the closest possible value at or below the requested value.

Parameters
[in]power

Desired radio output power, in deci-dBm.

[in]persistent

A flag to instruct the stack to save the power setting in persistent or not.

Note

  • Care should be taken when using this API on a running network, because it directly impacts the established link qualities neighboring nodes have with the node on which it is called. This can lead to disruption of existing routes and erratic network behavior.

Returns

  • An EmberStatus value indicating the success or failure of the command. Failure indicates that the requested power level is out of range.


Definition at line 353 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetRadioPower#

int16_t emberGetRadioPower (void )

Get the radio output power of the current network at which a node is operating. This might be different to what you set using emberSetRadioPower because the radio has a finite power resolution, and emberSetRadioPower must approximate to the closest possible value at or below the requested value. This API however returns with the actual setting.

Parameters
N/A

Returns

  • Current radio output power, in deci-dBm.


Definition at line 363 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberSetRadioPowerMode#

EmberStatus emberSetRadioPowerMode (bool radioOn)

Allow the application to turn the radio on/off. This API is intended for use with direct devices only.

Parameters
[in]radioOn

If this parameter is true, the radio is turned on, otherwise it's turned off.

Returns

  • An EmberStatus value indicating the success or failure of the command. Failure indicates that the node type is a type other than EMBER_DIRECT_DEVICE.


Definition at line 375 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberSetUnencryptedPacketsAcceptance#

EmberStatus emberSetUnencryptedPacketsAcceptance (bool accept)

Set if the stack should forward unencrypted messages to the application.

Parameters
[in]accept

If this parameter is true, unencrypted messages are forwarded to the application. They are not if this parameter is false.

Returns


Definition at line 388 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberSetMacParams#

EmberStatus emberSetMacParams (int8_t ccaThreshold, uint8_t maxCcaAttempts, uint8_t minBackoffExp, uint8_t maxBackoffExp, uint16_t ccaBackoff, uint16_t ccaDuration, uint8_t maxRetries, uint32_t csmaTimeout, uint16_t ackTimeout)

Set the MAC layer transmission parameters.

Parameters
[in]ccaThreshold

The CCA RSSI threshold, in dBm, above which the channel is considered 'busy'. This parameter is by default set to EMBER_RADIO_CCA_THRESHOLD.

[in]maxCcaAttempts

The maximum number of clear channel assessment attempts that are performed prior to fail to transmit a packet with EMBER_PHY_TX_CCA_FAIL status. This parameter is set by default to 4. If this parameter is set to 0, the CCA assessment shall not be performed.

[in]minBackoffExp

The backoff exponent used if the initial channel clear assessment fails. This parameter is set by default to 3. Note: this is meaningful only if the checkCca parameter is set to true.

[in]maxBackoffExp

The backoff exponent used if the final channel clear assessment fails. This parameter is set by default to 5. Note: this is meaningful only if the checkCca parameter is set to true.

[in]ccaBackoff

The backoff unit period in microsecond. It is multiplied by the random backoff exponential controlled by minBackoffExp and maxBackoffExp to determine the overall backoff period. This parameter is set by default to the PHY symbol time in microseconds multiplied by 20.

[in]ccaDuration

The minimum desired CCA check duration in microseconds. This parameter is set by default to the PHY symbol time in microseconds multiplied by 8.

[in]maxRetries

The number of transmission retries that is performed if no acknowledgment was received. This parameter is set by default to 3 (which means that a total of 4 transmission attempts will be performed).

[in]csmaTimeout

An overall timeout in microsecond time base for the the CSMA operations. This value is set by default to 0 which means that no timeout is imposed.

[in]ackTimeout

The ack timeout in microseconds after which the transmitting gives up waiting for an acknowledgment. This parameter is set by default to (EMBER_MAC_ACK_TIMEOUT_MS * 1000).

Note

  • The CSMA/CA (CCA) values are directly used in RAIL's RAIL_CsmaConfig_t and further information can be found in the RAIL API documentation.

Returns

  • An EmberStatus value indicating whether the MAC parameters were successfully set or the reason of failure.


Definition at line 445 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberMacGetParentAddress#

EmberStatus emberMacGetParentAddress (EmberMacAddress * parentAddress)

Retrieve the parent address. This API can be invoked only for nodes of EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE type.

Parameters
N/AparentAddress

Returns


Definition at line 462 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberStackIdleTimeMs#

uint32_t emberStackIdleTimeMs (uint16_t * currentStackTasks)

Return the time in milliseconds the stack could idle for.

Parameters
[in]currentStackTasks

A pointer to an integer that is written with the active stack tasks at the time of the API call.

Returns

  • Allowed idle time in milliseconds.


Definition at line 471 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetInt32uMillisecondTick#

uint32_t emberGetInt32uMillisecondTick (void )

Return the current time in milliseconds.

Parameters
N/A

Returns

  • Current time in milliseconds.


Definition at line 477 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberCurrentStackTasks#

uint16_t emberCurrentStackTasks (void )

Return a bitmask indicating the stack's current tasks.

Parameters
N/A

The mask EMBER_HIGH_PRIORITY_TASKS defines which tasks are high-priority. Devices should not sleep if any high-priority tasks are active. Active tasks that are not high-priority are waiting for messages to arrive from other devices. If there are active tasks, but no high-priority ones, the device may sleep but should periodically wake up and call emberPollForData() to receive messages. Parents will hold messages for EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS milliseconds before discarding them.

Returns

  • A bitmask of the stack's active tasks.


Definition at line 492 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberOkToNap#

bool emberOkToNap (void )

Indicate whether the stack is currently in a state with no high-priority tasks and may sleep.

Parameters
N/A

Tasks may be expecting incoming messages, in which case the device should periodically wake up and call emberPollForData() to receive messages. This function can only be called when the node type is EMBER_STAR_SLEEPY_END_DEVICE.

Returns

  • true if the application may sleep but the stack may be expecting incoming messages.


Definition at line 505 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberOkToHibernate#

bool emberOkToHibernate (void )

Indicate whether the stack currently has any pending tasks.

Parameters
N/A

If no tasks are pending , emberTick() does not need to be called until next stack API function is called. This function can only be called when the node type is EMBER_STAR_SLEEPY_END_DEVICE.

Returns

  • true if the application may sleep for as long as it wishes.


Definition at line 515 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetEui64#

uint8_t * emberGetEui64 (void )

Return the EUI64 ID of the local node.

Parameters
N/A

Returns

  • The 64-bit ID.


Definition at line 521 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberIsLocalEui64#

bool emberIsLocalEui64 (EmberEUI64 eui64)

Determine whether eui64 is the local node's EUI64 ID. EUI64 is easily accessible in SoC mode, but in Host-NCP, the address is stored on the NCP. This API can be used on the Host to compare a value with the locally stored one.

Parameters
[in]eui64

An EUI64 ID.

Returns

  • true if eui64 is the local node's ID, otherwise false.


Definition at line 532 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetNodeId#

EmberNodeId emberGetNodeId (void )

Return the 16-bit node ID of local node on the current network.

Parameters
N/A

Returns

  • The 16-bit ID. Byte order is little endian.


Definition at line 538 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetPanId#

EmberPanId emberGetPanId (void )

Return the local node's PAN ID of the current network.

Parameters
N/A

Returns

  • The PAN ID.


Definition at line 544 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetNodeType#

EmberNodeType emberGetNodeType (void )

Return an EmberNodeType value indicating the type of the node.

Parameters
N/A

Returns

  • The node type.


Definition at line 550 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetParentId#

EmberNodeId emberGetParentId (void )

Return the parent's node ID.

Parameters
N/A

Returns

  • The parent's node ID.


Definition at line 556 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

emberGetVersionInfo#

EmberStatus emberGetVersionInfo (uint16_t * platform_version, uint16_t * connect_stack_version, uint32_t * bootloader_version)

Get the Platform, Stack and bootloader versions all at once. The version format are not all the same. Please refer to the corresponding documentation to handle the information correctly. The Platform version corresponds to the deprecated GSDK version.

Parameters
N/Aplatform_version
N/Aconnect_stack_version
N/Abootloader_version

Returns

  • EMBER_SUCCESS if successful


Definition at line 564 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

Macro Definition Documentation#

EMBER_HIGH_PRIORITY_TASKS#

#define EMBER_HIGH_PRIORITY_TASKS
Value:
  (EMBER_OUTGOING_MESSAGES | EMBER_INCOMING_MESSAGES | EMBER_RADIO_IS_ON)

A mask of the tasks that prevent a device from sleeping.


Definition at line 44 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h

EMBER_INVALID_CHANNEL#

#define EMBER_INVALID_CHANNEL
Value:
65535

Invalid channel number.


Definition at line 51 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/stack-info.h