An instance of this structure is passed to emberMessageSentHandler(). It describes the outgoing packet.
Public Attribute Documentation#
options#
EmberMessageOptions EmberOutgoingMessage::options
An EmberMessageOptions value indicating the options used for transmitting the outgoing message.
destination#
EmberNodeId EmberOutgoingMessage::destination
An EmberNodeId value indicating the destination short ID.
tag#
uint8_t EmberOutgoingMessage::tag
A tag value the application can use to match emberMessageSend() calls to the corresponding emberMessageSentHandler() calls.
length#
EmberMessageLength EmberOutgoingMessage::length
An EmberMessageLength value indicating the length in bytes of the incoming message.
ackRssi#
int8_t EmberOutgoingMessage::ackRssi
The RSSI in dBm of the ACK corresponding to this message. This field is meaningful only if EMBER_OPTIONS_ACK_REQUESTED flag is set in the options field.
timestamp#
uint32_t EmberOutgoingMessage::timestamp
The millisecond system time returned by ::sl_sleeptimer at the time the sync word was transmitted.