Edit

Proprietary Radio Configurator Guide#

Note: This section replaces AN1253: EFR32 Radio Configurator Guide. Further updates to this application note will be provided here.

This document describes the Radio Configurator tool provided as part of Simplicity Studio® for Proprietary applications. With the help of the Radio Configurator, users can create standard or custom radio configurations for their RAIL- or Connect-based radio applications. This document explains the role of each item in the configuration.

If you are working with Proprietary SDK 2.7.n in Simplicity Studio 4, see AN971: EFR32 Radio Configurator Guide for RAIL in Simplicity Studio 4.