Modules#
Command Line Interface#
This module includes functions that control the Thread stack's execution.
Typedefs#
Pointer is called to notify about Console output.
Functions#
Initialize the CLI module.
Is called to feed in a console input line.
Set a user command table.
Write a number of bytes to the CLI console as a hex string.
Write formatted string to the CLI console.
Write error code to the CLI console.
Callback to write the OpenThread Log to the CLI console.
Callback to allow vendor specific commands to be added to the user command table.
Typedef Documentation#
otCliOutputCallback#
typedef int(* otCliOutputCallback) (void *aContext, const char *aFormat, va_list aArguments) )(void *aContext, const char *aFormat, va_list aArguments)
Pointer is called to notify about Console output.
Type | Direction | Argument Name | Description |
---|---|---|---|
[out] | aContext | A user context pointer. | |
[in] | aFormat | The format string. | |
[in] | aArguments | The format string arguments. |
Returns
Number of bytes written by the callback.
Function Documentation#
otCliInit#
void otCliInit (otInstance * aInstance, otCliOutputCallback aCallback, void * aContext)
Initialize the CLI module.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
otCliOutputCallback | [in] | aCallback | A callback method called to process CLI output. |
void * | [in] | aContext | A user context pointer. |
otCliInputLine#
void otCliInputLine (char * aBuf)
Is called to feed in a console input line.
Type | Direction | Argument Name | Description |
---|---|---|---|
char * | [in] | aBuf | A pointer to a null-terminated string. |
otCliSetUserCommands#
otError otCliSetUserCommands (const otCliCommand * aUserCommands, uint8_t aLength, void * aContext)
Set a user command table.
Type | Direction | Argument Name | Description |
---|---|---|---|
const otCliCommand * | [in] | aUserCommands | A pointer to an array with user commands. |
uint8_t | [in] | aLength |
|
void * | [in] | aContext |
|
otCliOutputBytes#
void otCliOutputBytes (const uint8_t * aBytes, uint8_t aLength)
Write a number of bytes to the CLI console as a hex string.
Type | Direction | Argument Name | Description |
---|---|---|---|
const uint8_t * | [in] | aBytes | A pointer to data which should be printed. |
uint8_t | [in] | aLength |
|
otCliOutputFormat#
void otCliOutputFormat (const char * aFmt, ... )
Write formatted string to the CLI console.
Type | Direction | Argument Name | Description |
---|---|---|---|
const char * | [in] | aFmt | A pointer to the format string. |
... | [in] | A matching list of arguments. |
otCliAppendResult#
void otCliAppendResult (otError aError)
Write error code to the CLI console.
Type | Direction | Argument Name | Description |
---|---|---|---|
otError | [in] | aError | Error code value. |
If the aError
is OT_ERROR_PENDING
nothing will be outputted.
otCliPlatLogv#
void otCliPlatLogv (otLogLevel aLogLevel, otLogRegion aLogRegion, const char * aFormat, va_list aArgs)
Callback to write the OpenThread Log to the CLI console.
Type | Direction | Argument Name | Description |
---|---|---|---|
otLogLevel | [in] | aLogLevel | The log level. |
otLogRegion | [in] | aLogRegion | The log region. |
const char * | [in] | aFormat | A pointer to the format string. |
va_list | [in] | aArgs | va_list matching aFormat. |
otCliVendorSetUserCommands#
void otCliVendorSetUserCommands (void )
Callback to allow vendor specific commands to be added to the user command table.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Available when OPENTHREAD_CONFIG_CLI_VENDOR_COMMANDS_ENABLE
is enabled and OPENTHREAD_CONFIG_CLI_MAX_USER_CMD_ENTRIES
is greater than 1.