Modules#

otRadioTimeStats

Radio Statistics#

Typedefs#

typedef struct otRadioTimeStats

Contains the statistics of radio.

Functions#

otRadioTimeStatsGet(otInstance *aInstance)

Gets the radio statistics.

void
otRadioTimeStatsReset(otInstance *aInstance)

Resets the radio statistics.

Typedef Documentation#

otRadioTimeStats#

typedef struct otRadioTimeStats otRadioTimeStats

Contains the statistics of radio.


Function Documentation#

otRadioTimeStatsGet#

const otRadioTimeStats * otRadioTimeStatsGet (otInstance * aInstance)

Gets the radio statistics.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

The radio statistics include the time when the radio is in TX/RX/Sleep state. These times are in units of microseconds. All times are calculated from the last reset of radio statistics.

Returns


otRadioTimeStatsReset#

void otRadioTimeStatsReset (otInstance * aInstance)

Resets the radio statistics.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

All times are reset to 0.