Configuration structure for a channel.
Public Attributes#
Select if channel priority is in the high or default priority group with respect to arbitration.
Select if interrupt will be enabled for channel (triggering interrupt handler when dma_done signal is asserted).
Channel control specifying the source of DMA signals.
User definable callback handling configuration.
Public Attribute Documentation#
highPri#
bool DMA_CfgChannel_TypeDef::highPri
Select if channel priority is in the high or default priority group with respect to arbitration.
Within a priority group, lower numbered channels have higher priority than higher numbered channels.
158
of file platform/emlib/inc/em_dma.h
enableInt#
bool DMA_CfgChannel_TypeDef::enableInt
Select if interrupt will be enabled for channel (triggering interrupt handler when dma_done signal is asserted).
It should normally be enabled if using the callback feature for a channel, and disabled if not using the callback feature.
166
of file platform/emlib/inc/em_dma.h
select#
uint32_t DMA_CfgChannel_TypeDef::select
Channel control specifying the source of DMA signals.
If accessing peripherals, use one of the DMAREQ_nnn defines available for the peripheral. Set to 0 for memory-to-memory DMA cycles.
173
of file platform/emlib/inc/em_dma.h
cb#
DMA_CB_TypeDef* DMA_CfgChannel_TypeDef::cb
User definable callback handling configuration.
Refer to structure definition for details. The callback is invoked when specified DMA cycle is complete (when dma_done signal asserted). Callback is invoked in interrupt context, and should be efficient and non-blocking. Set to NULL to not use the callback feature. Note
Referenced structure is used by the interrupt handler, and must be available until no longer used. Thus, in most cases it should not be located on the stack.
189
of file platform/emlib/inc/em_dma.h