HFXO initialization structure.
Initialization values should be obtained from a configuration tool, application note or crystal data sheet.
Public Attributes#
Enable low-power mode.
Startup phase CTUNE (load capacitance) value.
Steady-state phase CTUNE (load capacitance) value.
Shunt steady-state current.
Startup XO core bias current trim.
Steady-state XO core bias current trim.
Peak detection threshold.
Timeout - shunt optimization.
Timeout - peak detection.
Timeout - steady-state.
Timeout - startup.
Oscillator mode.
Public Attribute Documentation#
lowPowerMode#
bool CMU_HFXOInit_TypeDef::lowPowerMode
Enable low-power mode.
3157
of file platform/emlib/inc/em_cmu.h
autoStartEm01#
bool CMU_HFXOInit_TypeDef::autoStartEm01
3158
of file platform/emlib/inc/em_cmu.h
autoSelEm01#
bool CMU_HFXOInit_TypeDef::autoSelEm01
3159
of file platform/emlib/inc/em_cmu.h
autoStartSelOnRacWakeup#
bool CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup
3160
of file platform/emlib/inc/em_cmu.h
ctuneStartup#
uint16_t CMU_HFXOInit_TypeDef::ctuneStartup
Startup phase CTUNE (load capacitance) value.
3161
of file platform/emlib/inc/em_cmu.h
ctuneSteadyState#
uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState
Steady-state phase CTUNE (load capacitance) value.
3162
of file platform/emlib/inc/em_cmu.h
regIshSteadyState#
uint8_t CMU_HFXOInit_TypeDef::regIshSteadyState
Shunt steady-state current.
3163
of file platform/emlib/inc/em_cmu.h
xoCoreBiasTrimStartup#
uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup
Startup XO core bias current trim.
3164
of file platform/emlib/inc/em_cmu.h
xoCoreBiasTrimSteadyState#
uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState
Steady-state XO core bias current trim.
3165
of file platform/emlib/inc/em_cmu.h
thresholdPeakDetect#
uint8_t CMU_HFXOInit_TypeDef::thresholdPeakDetect
Peak detection threshold.
3166
of file platform/emlib/inc/em_cmu.h
timeoutShuntOptimization#
uint8_t CMU_HFXOInit_TypeDef::timeoutShuntOptimization
Timeout - shunt optimization.
3167
of file platform/emlib/inc/em_cmu.h
timeoutPeakDetect#
uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect
Timeout - peak detection.
3168
of file platform/emlib/inc/em_cmu.h
timeoutSteady#
uint8_t CMU_HFXOInit_TypeDef::timeoutSteady
Timeout - steady-state.
3169
of file platform/emlib/inc/em_cmu.h
timeoutStartup#
uint8_t CMU_HFXOInit_TypeDef::timeoutStartup
Timeout - startup.
3170
of file platform/emlib/inc/em_cmu.h
mode#
CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode
Oscillator mode.
3176
of file platform/emlib/inc/em_cmu.h