VMON initialization structure.
Public Attributes#
VMON channel to configure.
int
Trigger threshold (mV).
bool
Wake up from EM4H on rising edge.
bool
Wake up from EM4H on falling edge.
bool
Enable VMON channel.
bool
Disable IO0 retention when voltage drops below threshold (IOVDD only).
Public Attribute Documentation#
channel#
EMU_VmonChannel_TypeDef EMU_VmonInit_TypeDef::channel
VMON channel to configure.
Definition at line
1059
of file platform/emlib/inc/em_emu.h
threshold#
int EMU_VmonInit_TypeDef::threshold
Trigger threshold (mV).
Supported range is 1620 mV to 3400 mV.
Definition at line
1060
of file platform/emlib/inc/em_emu.h
riseWakeup#
bool EMU_VmonInit_TypeDef::riseWakeup
Wake up from EM4H on rising edge.
Definition at line
1061
of file platform/emlib/inc/em_emu.h
fallWakeup#
bool EMU_VmonInit_TypeDef::fallWakeup
Wake up from EM4H on falling edge.
Definition at line
1062
of file platform/emlib/inc/em_emu.h
enable#
bool EMU_VmonInit_TypeDef::enable
Enable VMON channel.
Definition at line
1063
of file platform/emlib/inc/em_emu.h
retDisable#
bool EMU_VmonInit_TypeDef::retDisable
Disable IO0 retention when voltage drops below threshold (IOVDD only).
Definition at line
1064
of file platform/emlib/inc/em_emu.h