Configuration structure for the alternate excitation.
Public Attribute Documentation#
altExMap#
LESENSE_AltExMap_TypeDef LESENSE_ConfAltEx_TypeDef::altExMap
Select alternate excitation mapping.
Definition at line
1232
of file platform/emlib/inc/em_lesense.h
AltEx#
LESENSE_AltExDesc_TypeDef LESENSE_ConfAltEx_TypeDef::AltEx[16]
Alternate excitation channel descriptors.
When altExMap==lesenseAltExMapALTEX, only the 8 first descriptors are used. In this mode they describe the configuration of LES_ALTEX0-7 pins. When altExMap==lesenseAltExMapACMP, all 16 descriptors are used. In this mode they describe the configuration of the 16 possible ACMP0-1 excitation channels. Please refer to the user manual for a complete mapping of routing. NOTE: Some parameters in the descriptors are not valid when altExMap==lesenseAltExMapACMP. Refer to the definition of the LESENSE_AltExDesc_TypeDef structure for details regarding which parameters are valid.
Definition at line
1247
of file platform/emlib/inc/em_lesense.h